Skip to main content
BillG
Associate II
May 31, 2023 2:25 PM UTC
Question

PMOD (or Arduino) Ethernet on STM32H747i-disco Board

Has anyone tried to get ethernet over PMOD or perhaps with Arduino working on the STM32747i discovery board? I need ethernet but modifying the solder bridges is not something I can do.

Maybe I could use the STMod+ expansion board and try the mikroBus connector?

Thanks.

-bill

This topic has been closed for replies.

1 reply

S.Ma
Principal
Jun 3, 2023 5:18 PM UTC

The remote ethernet are spi based, so probably low speed. The 10/100 ethernet of STM32 uses 10 wires and 25Mhz clock. If it is not a production project, the spi click will lower the complexity and development time.