Skip to main content
MGall.9
Visitor II
Jun 14, 2019 3:21 PM UTC
Question

PLL3 as I2C123 peripheral source clock on STM32H7

If the PLL3 is selected as I2C peripheral source clock, the Bits RCC_D2CCIP2R_I2C123SEL are not initialized correctly.

In function HAL_RCCEx_PeriphCLKConfig() the PLL3 R Divider gets updated but the clock selection is not set to "1". In my opinion, this should be fixed as written below:

original code:

 /*------------------------------ I2C1/2/3 Configuration ------------------------*/
 if(((PeriphClkInit->PeriphClockSelection) & RCC_PERIPHCLK_I2C123) == RCC_PERIPHCLK_I2C123)
 {
 /* Check the parameters */
 assert_param(IS_RCC_I2C123CLKSOURCE(PeriphClkInit->I2c123ClockSelection));
 
 if ((PeriphClkInit->I2c123ClockSelection )== RCC_I2C123CLKSOURCE_PLL3 )
 {
 if(RCCEx_PLL3_Config(&(PeriphClkInit->PLL3),DIVIDER_R_UPDATE)!= HAL_OK)
 {
 status = HAL_ERROR;
 }
 }
 
 else
 {
 __HAL_RCC_I2C123_CONFIG(PeriphClkInit->I2c123ClockSelection);
 }
 
 }

Fixed code:

 /*------------------------------ I2C1/2/3 Configuration ------------------------*/
 if(((PeriphClkInit->PeriphClockSelection) & RCC_PERIPHCLK_I2C123) == RCC_PERIPHCLK_I2C123)
 {
 /* Check the parameters */
 assert_param(IS_RCC_I2C123CLKSOURCE(PeriphClkInit->I2c123ClockSelection));
 
 if ((PeriphClkInit->I2c123ClockSelection )== RCC_I2C123CLKSOURCE_PLL3 )
 {
 if(RCCEx_PLL3_Config(&(PeriphClkInit->PLL3),DIVIDER_R_UPDATE)!= HAL_OK)
 {
 status = HAL_ERROR;
 }
 }
 
 __HAL_RCC_I2C123_CONFIG(PeriphClkInit->I2c123ClockSelection);
 
 }

I use the STM32Cube_FW_H7_V1.4.0 HAL

This topic has been closed for replies.