Skip to main content
Sean1
Visitor II
December 14, 2018
Question

PLL initialization defect on Nucleo F767ZI

  • December 14, 2018
  • 0 replies
  • 559 views

In main.c, SystemClock_Config(), the PLL is set up as follows:

...

 RCC_OscInitStruct.PLL.PLLM = 25;

 RCC_OscInitStruct.PLL.PLLN = 400;  

...

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

...

The implication is that the clock is 25MHz, and being divided down to 1MHz as input to the VCO. However, by default the input clock is actually 8MHz supplied by the ST-Link. The effect is to run the PLL CLK at 64MHz, instead of the implied 200MHz.

Note that this is definitely wrong, not just a subjective decision to run the clock slower, because the reference manual indicates that the VCO input frequency range should be between 1MHz and 2MHz.

This topic has been closed for replies.