Skip to main content
Jur Div
Associate II
May 16, 2018 5:54 PM UTC
Question

PlatformIO stm32cube framework isn't complete

Posted on May 16, 2018 at 19:54

I am using

https://platformio.org/platformio-ide

to program the STM32 F7 discovery board. The STM32Cube package is in the PlatformIO's framework registry and HAL&CMSIS drivers are working out of the box without problems.

Since I am not using any RTOS and only trying small examples at the moment, I noticed that the

http://docs.platformio.org/en/latest/frameworks/stm32cube.html

of stm32cube is not complete. It (for example) doesn't include BSP drivers and it doesn't include STemWin library.

Why is that? At the moment I am using manually downloaded

http://www.st.com/en/embedded-software/stm32cubef7.html

package and including BSP drivers manually and unsucessfully including STemWin library manually as well. It involves a lot of 'hacking' around (include paths, compilation options etc.), which doesn't make sense- since the stm32cube (and PIO library manager) was designed to 'make developer's life easier'

It's confusing that the PIO version of stm32cube is not the same as the 'official' one. If there's some reason I missed in all this? Would it be possible to make BSP and Middlewares (STemWin) 'official' libraries, so you could add them via PIO Library Manager?

Also, the

https://platformio.org/lib/show/2210/BSP_DISCO_F746NG

of the BSP library is compatible only with mbed framework. Why couldn't one use it only with stm32cube framework (HAL)...? I could find and official or complete STemWin library in the PlatformIO library registry.

Thank you for help,

Jur

#stm32f746-discovery #stm32-f7 #platformio #cube
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
May 18, 2018 9:01 AM UTC
Posted on May 18, 2018 at 11:01

I'd say you should ask these questions at Platformio.

JW