Skip to main content
Associate
Jul 29, 2024 4:54 PM UTC
Question

PD3.1 EPR sniffing on STM32G071B-DISCO

Hi all,

Could anyone advise the current status of EPR support on the UCPD software? Thanks.

Best Regards

EY

This topic has been closed for replies.

4 replies

LLECH.1
ST Employee
Aug 5, 2024 7:36 AM UTC

Hello Ey,

The STM32G071B-DISCO  doesn't have the necessary hardware equipment to support EPR.

Best Regards,

Lucas

LLECH.1
ST Employee
Aug 5, 2024 3:49 PM UTC

Hello,

By "doesn't have the necessary hardware equipment" I mean that STM32G071RB-DISCO can support up to 26V. Beyond this value you could damage the device.

 

Best Regards

ey_itAuthor
Associate
Aug 5, 2024 6:47 PM UTC

Dear Lucas,

Many thanks for following up my query. I was aware of the 26V limit but still would like to know whether EPR voltages below 26V would be supported (in my case it’s 24V with AVS). If not could I do such PD3.1 sniffing with ST TCPP evaluation kits?

 

Thanks again for your help.

Best Regards

Edwin

LLECH.1
ST Employee
Aug 6, 2024 6:55 AM UTC

Hello Ey,

Unfortunately EPR voltages below 26V are not supported either since software don't handle it. To detect EPR voltages, STM32G071RB-DISCO must ask for EPR source capabilities which it doesn't. Thus, you won't be able to detect EPR voltages.

Br,

Lucas