Skip to main content
Associate III
May 29, 2025 5:23 AM UTC
Solved

PA0_C/PA1_C/PC2_C/PC3_C[STM32H743XGH6]

PA0_C/PA1_C/PC2_C/PC3_C
What is the base address for the above four GPIOs that can be set?

Also, do you have the following understanding about the above 4 pins?
Pxy_C can be set to a pin of the same function or another function by controlling an analog switch.

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
May 29, 2025 8:13 AM UTC

https://community.st.com/t5/stm32-mcus-products/confusion-about-c-pins-pa0-c-behavior-and-functionality/m-p/787244?search-action-id=56405571184&search-result-uid=787244

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

2 replies

Andrew Neil
Andrew NeilBest answer
Super User
May 29, 2025 8:13 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NiMAuthor
Associate III
Jun 11, 2025 10:32 AM UTC

Thank you very much.

I understand, there is no separate configuration register for Pxy_C, you are talking about whether or not it is connected via a switch to the Pxy's pins.