Skip to main content
New.Fish
Associate III
Jul 4, 2021 11:44 AM UTC
Question

P-L496_Cell02 can't find SIM

There are eSIM and Mirco_SIM in the Modem board, but it keep report:

CST_modem_sim_init : Can't find sim on current slot. Increment sim slot.    

CST_modem_sim_init : No more sim slot, no SIM found. Retry...

     

Any suggestion?

This topic has been closed for replies.

6 replies

S.RA
ST Employee
Jul 5, 2021 10:21 AM UTC

Dear @New.Fish

I understand that you have inserted a SIM card in the micros SIM slot of the Modem Board. Can you share the trace from the terminal so that we can make more detail analysis of the issue?

Thanks a lot

Best Regards

Solofo

New.Fish
New.FishAuthor
Associate III
Jul 5, 2021 12:58 PM UTC

Hello,

Please check my log file

Regards

S.RA
ST Employee
Jul 5, 2021 6:42 PM UTC

Hello,

Can you confirm if you have inserted a SIM card in the micoro SIM socket slot?

If this is the case, then I suggest to update first the Modem FW to be compatible with X-CUBE-CELLULAR.

The instruction to update the Modem Firmware is provided in the

\STM32CubeExpansion_CELLULAR_V6.0.0\Utilities\Modem_FW\BG96\

Let me know if you still have issue.

Best Regards

Solofo

New.Fish
New.FishAuthor
Associate III
Jul 12, 2021 9:52 AM UTC

By default, this demo software is connected to eSIM or MicroSIM?

It suppose have 3 months of free usage, I follow the instruction, but I can't make it work, what's wrong?

New.Fish
New.FishAuthor
Associate III
Jul 12, 2021 3:47 AM UTC

Hello,

I try to use "QFlash" to update the Cellular firmware, the "QFlash" get problem with Win7 and Win 10 PC, I contact Quectel FAE this stage.

Reagrsd