Skip to main content
Senior
Jan 23, 2026 7:54 AM UTC
Solved

Output gain set is omitted in WM8904_Init()

Hi,

// WM8904.c
int32_t WM8904_Init(WM8904_Object_t *pObj, WM8904_Init_t *pInit)
 // ...
 if ((WM8904_CurrentDevices & WM8904_OUT_HEADPHONE) == WM8904_OUT_HEADPHONE)
 {
 ret += WM8904_SetVolume(pObj, VOLUME_OUTPUT, (uint8_t)pInit->Volume);
 }

 // ...
 
 /* Store current devices */
 WM8904_CurrentDevices = (pInit->OutputDevice | pInit->InputDevice);

 in line 4, WM8904_CurrentDevices is still 0, so the gain is not set.

I'd change the line this way:

 if ((pInit->OutputDevice & WM8904_OUT_HEADPHONE) == WM8904_OUT_HEADPHONE)
 {
 ret += WM8904_SetVolume(pObj, VOLUME_OUTPUT, (uint8_t)pInit->Volume);
 }

 

Saket_OmBest answer
ST Technical Moderator
Jan 23, 2026 3:03 PM UTC

Hello @ERROR 

The issue has been solved and released on Github. Please check the link below:

STMicroelectronics/stm32-wm8904 at 195857c3b70fc582fc534df5c8e5d3b2a1c40bb4

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

2 replies

ST Technical Moderator
Jan 23, 2026 10:50 AM UTC

Hello @ERROR 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 225790 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Saket_OmBest answer
ST Technical Moderator
Jan 23, 2026 3:03 PM UTC

Hello @ERROR 

The issue has been solved and released on Github. Please check the link below:

STMicroelectronics/stm32-wm8904 at 195857c3b70fc582fc534df5c8e5d3b2a1c40bb4

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om