Skip to main content
SWood.4
Associate III
Sep 23, 2022 7:55 PM UTC
Question

OTA firmware update for a Nucleo F746.

*Edited, I had a long question about why the code wasn't working. I was using an example based on Embetronicx. Here is the git location for his example. https://github.com/Embetronicx/Tutorials/tree/ETX_Bootloader_3.0/Microcontrollers/STM32/STM32F7xx/Bootloader_Example

I found a video series from ST on building a bootloader also. The ST example is significantly different than the Embetronicx example. Embetronicx has good information and it may be good to use. I'm not sure based on the other info I'm finding.

So my question is; what is the best simple method of an OTA bootloader? Do you have links or examples?

Thanks

 

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Sep 24, 2022 12:03 AM UTC

Well typically the tool-chain doesn't send the .BIN, it works off the .ELF, and that can be sectional and sparse. Perhaps use objcopy or fromelf to inspect. The .HEX might be more record based.

I might suggest

Instrument the code, outputting progress and sums

Get a Hard Fault Handler that outputs actionable data

Step the transition code

Avoid reconfiguring clocks, so don't teardown in SystemInit(), and just set SCB->VTOR =&__gfnVectors, then skip the SystemClock_Config()

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Sep 26, 2022 10:17 PM UTC

@Community member​ Why do you want to use this github example as a base for "OTA update"? UART is not a wireless ("air") interface.

SWood.4
SWood.4Author
Associate III
Sep 27, 2022 3:28 PM UTC

The embedded cell modem connected to the MCU has a UART interface. The connection from the server application to the MCU ends up like a serial connection to the PC. The cell modem and ethernet connections in the middle end up transparent to the applications on both ends. So I need a way to update firmware over a cellular VPN, with a UART connection.

My thought is for the server application to send a UART command so the MCU knows what follows is a firmware update, the MCU can save firmware to a FLASH location, do check sum , CRC etc. if its good, save a value at a location the bootloader checks so it knows new firmware is available, reset MCU, boot loader checks if new firmware is available, copies firmware to the Application area of the MCU, jumps to that location and runs it.

I had also thought about having two application areas, the bootloader would jump to the one with the higher number, most recent version. Then the MCU application updates the firmware for the "offline" application, next reset the newer one runs.

Let me know there is a better approach or an entirely better way of getting new firmware on a remote MCU. Thanks

Pavel A.
Sep 28, 2022 12:02 AM UTC

@Community member​ Your approach generally looks good and should work.

(recently I've seen this thing from inside; it has the same STM32F7 and a similar UART-connected wireless interface. The update process works exactly as you describe, except that it pulls updates from a cloud web server).

> I had also thought about having two application areas, the bootloader would jump to the one with the higher number

This won't work unless you manage to make position independent binaries. By default the CubeIDE will produce code located at specific address, it won't run in place at a different address.

Tesla DeLorean
Guru
Sep 26, 2022 10:30 PM UTC

Dramatically editing top posts removing the original question is unhelpful.

Open a new question, or add a new post to the thread to take it in a different direction.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..