osTimer Callback Context and Priority
I'm using STM32L152RET with FreeRTOS (cmsis wrapper) for my product.
I'm struggling to understand the priority and context of the freertos "timer interrupt". We use a cmsis wrapper (code generated from CubeMX) and the freertos based timer task is referred to as an "osTimer" in CMSIS wrapper.
Can someone tell me which of this is correct ? The callback function triggered from the os timer
- runs with the priority of the timer task ?
- runs with the priority of the task from which the timer was created ?
- is in interrupt context and hence always the highest priority ?
To share more information :
Our systems has 3 tasks :
- Comm task (for cellular modem) (medium priority)
- AV task ( low priority ) - for scheduling LED and Buzzer PWM
- Service Task (High priority) - central event handling mechanism
- Timer Task ( (Highest - 1) priority as set up by freertos internal defines )
There is a case of priority inversion that I notice in the following scenario -
- The AV TASK calls appropriate LED and Buzzer Drivers and suspends on osTimer
- The Com Task starts executing from a separate event
- When the OS timer times out, it interrupts and triggers a callback function
- The Callback function does not pend the lower priority Comm Task
- It only executes after the comm task has completed it's execution
- This causes the LED and Buzzer pattern to be distorted
The timer callback has the code to handle the pwm for of LED and Buzzer and in turn change the brightness and tone.
I would assume that the timer task has the highest priority and it gets the CPU time,and thus it's callback function will run at the same context and get CPU time, but that does not happen.
Any suggestions on how I can handle this or corrections in my theory ?
Thanks in advance