Skip to main content
Senior
Jul 3, 2024 2:42 PM UTC
Solved

OPUS EXAMPLE

i have compiled opus lib on H5. but i can not decode data.

this is my init function and works fine.  
 DecConfigOpus.channels = 2;
 DecConfigOpus.ms_frame = 20;
 DecConfigOpus.sample_freq = 48000;
 uint32_t dec_size = DEC_Opus_getMemorySize(&DecConfigOpus);
 DecConfigOpus.pInternalMemory = (uint8_t *)malloc(dec_size);
 int opus_err;
 if (DEC_Opus_Init(&DecConfigOpus, &opus_err) != OPUS_SUCCESS)
 {
 printf("ERROR! DEC_Opus_Init()\r\n");
 break;
 }
and in decode function first time return 960 and then -4.
int packetSize = 80; // Adjust based on your actual packet size
for (int i = 0; i < sizeof(music); i += packetSize)
{
 int x = DEC_Opus_Decode((uint8_t*)&music[i], packetSize, DecConfigOpus.pInternalMemory);
 if (x < 0)
 {
 printf("Error decoding packet at index %d: %d\n", i, x);
 break; // Exit the loop or handle error as appropriate
 }
 else 
 {
 printf("Decoded packet at index %d, x = %d\n", i, x);
 }
}
 
This topic has been closed for replies.
nimaltdBest answer
Senior
Jul 4, 2024 6:13 AM UTC

i think i found the problem, my start point of data was wrong. ( skip header/tag did not work property)

how to find the packetSize? 

 

2 replies

mƎALLEm
ST Technical Moderator
Jul 3, 2024 2:47 PM UTC

Hello @nimaltd ,

A gentle reminder on how to post a thread in this community mainly on how to share a code source. I suggest to review these recommendations.

Thank your for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
nimaltdAuthorBest answer
Senior
Jul 4, 2024 6:13 AM UTC

i think i found the problem, my start point of data was wrong. ( skip header/tag did not work property)

how to find the packetSize?