Skip to main content
LROME.1
Visitor II
May 9, 2022 3:06 PM UTC
Question

On L151, SPI Half duplex in pooling mode, HAL generate nb word length clock cycle more while reading

Hi FAEs and the community,

On a L151 the SPI block has a strange behavior.

Some time to time it generates 8 clock cycles more on a read (if I use size 8 bits) or 16 bits (if I use size 16 bits).

My target is a 16 bits based half duplex SPI device.

Thus it introduces a shift on the next read and messing up everything...

I use the HAL (HAL_SPI_Receive and HAL_SPI_Transmit).

Withe a prescaler at SPI_BAUDRATEPRESCALER_128 (means 250Khz) I have few errors.

If I go up to SPI_BAUDRATEPRESCALER_64 (in spec according the stm32l1xx_hal_spi.c file) then the error is immediate...

Does someone has seen this behavior before ? Is there a fix ?

Is there a way to flush the RX fifo datas (if any) from this IP (and I have a work around) ?

Thanks a lot

Regards

Lionel.

This topic has been closed for replies.