OEMiROT_Boot with NUCLEO-H563ZI and Visual Studio Code with STM32Cube_FW_H5_V1.7.0 error/not function
Hello to all,
I follow the creation of OEMiROT_Boot, app secure, app not secure with NUCLEO-H563ZI like suggested into https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_STM32CubeMX_OEMiRoT_Boot_path_on_STM32H563.
I want to use Visual studio Code with extension STM32CubeIDE.
Follwing the instructions into the web page “:How_to_start_with_STM32CubeMX_OEMiRoT_Boot_path_on_STM32H563.” I have to compile the OEMiROT_Boot, if I import the project OEMiROT_Boot from STM32Cube_FW_H5_V1.7.0 for NUCLEO-H563ZI, into vs code there are error I have to copy “stm32h5xx_bl2.ld” to utput.ld into the same folder to let vs code to import without error but it’s not possible to compile the project, then I’ll compile the other with keil without problem.
After I’ve follwed the list of operation to do but at the point “ 5. Debug Authentication configuration” I cannot select configure (into the project configuratione of MXCube I’ll try to create a project KEIL and CMAKE without lack because I can compile OEMiROT_Boot only with keil)

Then are there solution to avoid this problem?
STM32CubeMx is

Then, are there solution to avoid this problem?
Best Regards
Gianluca