Skip to main content
Nukat
Associate
Aug 8, 2019 2:10 PM UTC
Question

Nucleo-STM32F429ZI Ethernet + LWIP (RAW API) - doesn't work.

I've got a project in which I have to communicate by Ethernet (TCP) Nucleo-STM32F429ZI with PC. STM32 will be sending the data from sensor periodically. I'm using STM32CubeIDE with built in CubeMX. I've connected the STM32 and the PC with a crossed cable. I configured it without RTOS, only using LwIP in RAW API mode with static IP addresses. I’m calling the MX_LWIP_Process() function in while loop.

My problem is that I can't receive ping response from STM32 and I’m getting the “Destination Host Unreachable�? message. I've tried every configuration and advice I found on forums and it didn't work. I've tried to adapt my project configuration to that from the example for my board (LwIP_HTTP_Server_Netconn_RTOS which works and response) but it didn't work too. 

As I'm debugging my project I can receive the ARP frame with request for IP address and I can see in debugger that the output frame is correct but as the whole payload is passed to "HAL_ETH_TransmitFrame" function, the output/response frame is gone, I can't see it in the Wireshark. I've checked the pinout configuration for the Ethernet peripheral and the configuration addresses. I really don't know what I’m missing. 

I've got auto-negotiation enabled in ETH CubeMX and I've change the PHY address from default 1 to 0 and PHY Link down inturrupt from 0xB to 0x10 according to datasheet (I hope it's correct).

Below I pasted my configuration for Ethernet PHY (LAN8742A):

/* LAN8742A_PHY_ADDRESS Address*/

#define LAN8742A_PHY_ADDRESS           0U

/* PHY Reset delay these values are based on a 1 ms Systick interrupt*/

#define PHY_RESET_DELAY                 ((uint32_t)0x00000FFFU)

/* PHY Configuration delay */

#define PHY_CONFIG_DELAY                ((uint32_t)0x00000FFFU)

#define PHY_READ_TO                     ((uint32_t)0x0000FFFFU)

#define PHY_WRITE_TO                    ((uint32_t)0x0000FFFFU)

/* Section 3: Common PHY Registers */

#define PHY_BCR                         ((uint16_t)0x00U)    /*!< Transceiver Basic Control Register   */

#define PHY_BSR                         ((uint16_t)0x01U)    /*!< Transceiver Basic Status Register    */

#define PHY_RESET                       ((uint16_t)0x8000U)  /*!< PHY Reset */

#define PHY_LOOPBACK                    ((uint16_t)0x4000U)  /*!< Select loop-back mode */

#define PHY_FULLDUPLEX_100M             ((uint16_t)0x2100U)  /*!< Set the full-duplex mode at 100 Mb/s */

#define PHY_HALFDUPLEX_100M             ((uint16_t)0x2000U)  /*!< Set the half-duplex mode at 100 Mb/s */

#define PHY_FULLDUPLEX_10M              ((uint16_t)0x0100U)  /*!< Set the full-duplex mode at 10 Mb/s  */

#define PHY_HALFDUPLEX_10M              ((uint16_t)0x0000U)  /*!< Set the half-duplex mode at 10 Mb/s  */

#define PHY_AUTONEGOTIATION             ((uint16_t)0x1000U)  /*!< Enable auto-negotiation function     */

#define PHY_RESTART_AUTONEGOTIATION     ((uint16_t)0x0200U)  /*!< Restart auto-negotiation function    */

#define PHY_POWERDOWN                   ((uint16_t)0x0800U)  /*!< Select the power down mode           */

#define PHY_ISOLATE                     ((uint16_t)0x0400U)  /*!< Isolate PHY from MII                 */

#define PHY_AUTONEGO_COMPLETE           ((uint16_t)0x0020U)  /*!< Auto-Negotiation process completed   */

#define PHY_LINKED_STATUS               ((uint16_t)0x0004U)  /*!< Valid link established               */

#define PHY_JABBER_DETECTION            ((uint16_t)0x0002U)  /*!< Jabber condition detected            */

/* Section 4: Extended PHY Registers */

#define PHY_SR                          ((uint16_t)0x1FU)    /*!< PHY status register Offset                      */

#define PHY_SPEED_STATUS                ((uint16_t)0x0004U)  /*!< PHY Speed mask                                 */

#define PHY_DUPLEX_STATUS               ((uint16_t)0x0010U)  /*!< PHY Duplex mask                                 */

#define PHY_ISFR                        ((uint16_t)0x001DU)    /*!< PHY Interrupt Source Flag register Offset   */

#define PHY_ISFR_INT4                   ((uint16_t)0x0010U)  /*!< PHY Link down inturrupt       */ 

My whole project is in the attachment. If you need any additional information about the setup please ask. Thank you very much for any help.

This topic has been closed for replies.

2 replies

Geraldo Pereira
Associate III
Oct 19, 2020 7:36 PM UTC

Hi Nukat,

Did ou solve your problem? I´ve just bought a nucleo-F429Zi board to implement a socket project. What do you think? can I use this board? Will it support ethernet communication?

Thanks,

Geraldo.

MRMehrdad
Visitor II
Jun 29, 2022 11:56 AM UTC

your problem might be in platform setting section of LWIP