Skip to main content
Nagendra A Karmarkar
Visitor II
Nov 8, 2022 6:25 AM UTC
Question

Nucleo L433RC-P flash program (read/write data)

I want to store some data into flash (read/write)..i have no idea wheter it can be done with Nucleo L433RC-P DK. if possible plz share the example code

i tried with an example code (github - controllerstech F1, F4, H7 series) . but no use of it

This topic has been closed for replies.

2 replies

ST Technical Moderator
Nov 8, 2022 11:41 AM UTC

Hello @Nagendra A Karmarkar​ and welcome to the Community :)

You can use the available "Flash" example within STM32CubeL4 package:

STM32Cube_FW_L4_V1.17.2\Projects\NUCLEO-L432KC\Examples\FLASH\FLASH_WriteProtection

STM32CubeL4/Projects/NUCLEO-L452RE/Examples/FLASH at master · STMicroelectronics/STM32CubeL4 · GitHub

Hope this helps you!

When your question is answred, please close this thread by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Piranha
Principal III
Nov 8, 2022 7:12 PM UTC

> i have no idea wheter it can be done

Then try reading the reference manual!