Skip to main content
Associate
June 12, 2026
Solved

NUCLEO-H7S3L8 USB_OTG_HS Host Issue: TXERR during EP0 SETUP

  • June 12, 2026
  • 5 replies
  • 108 views

I am currently using the NUCLEO-H7S3L8 CN2 Type-C port as a USB_OTG_HS embedded PHY host/source.

The TCPP03 source path opens successfully, and both the USB stick attachment and port reset are working. After the reset, HPRT reads 0x00001005, which seems to indicate speed=HS and that the port is enabled.

However, during the first EP0 SETUP GET_DESCRIPTOR request:

  • HAL_HCD_HC_SubmitRequest() = HAL_OK

  • HAINT = 0x00000001

  • HCINT = 0x00000080

  • TXERR = 1

  • xfer_count = 0

The exact same issue occurs even during a raw HAL EP0 smoke test, prior to involving USBX/FileX.

I would like to verify the following points:

  1. What is the mandatory clock/power initialization sequence when using the USB_OTG_HS embedded PHY host on the H7S3L8?

  2. Is it acceptable to use HSI → PLL3Q for the USBPHYC clock, or is an HSE strictly required?

  3. What are the necessary settle/wait conditions after enabling USBHSREG?

  4. Are there any required CC/UCPD configurations for the CN2 Type-C/TCPP03 source setup, apart from the PM9 PWR_EN + TCPP03 provider gate?

  5. Is the state where HPRT = 0x00001005 and HCFG = 0x00000201 considered normal under these conditions?

Best answer by FBL

Hi ​@wooseong 

Apologies for the delayed response, and thank you for sharing the minimal firmware package.

This is very helpful. Can you confirm CDC_Standalone example in host mode is working as expected on the Nucleo H7S3?

I found two ST reference examples that may be useful as a baseline for the USB Host MSC path:

  • X-CUBE-AZRTOS-H7RS /Projects/STM32H7S78-DK/Applications/USBX/Ux_Host_MSC

  • STM32CubeH7RS /Projects/STM32H7S78-DK/Applications/USB_Host/MSC_RTOS

These examples are for STM32H7S78-DK, not NUCLEO-H7S3L8, but they should still help you compare the USB host, USBX, and MSC initialization sequence.

5 replies

wooseongAuthor
Associate
June 12, 2026

Update:

I tested the USBPHY reference clock and USB HS regulator related points suggested by similar H7RS/N6 USBPHYC issues.

Current HSI -> PLL3Q -> USBPHYC path:

  • USBPHY clock source: PLL3Q

  • USBREF forced/logged as 24 MHz

  • CCIPR1 = 0x00002a40

  • USBPHYCSEL = 0x00002000

  • USBREFCKSEL = 0x00000a00

  • USBHSREGEN = 1

  • USB33RDY = 1

  • GOTGCTL after HAL_HCD_Start() = 0x002c0000

However, the first EP0 SETUP still fails with:

  • HAINT = 0x00000001

  • HCINT = 0x00000080

  • TXERR = 1

  • xfer_count = 0

I also tested HSE-based USBPHYC clock presets.

HSE preset:

  • HSERDY = 0

  • PLL3RDY = 0

  • USBPHYC clock setup failed with HAL status 0x03

HSE bypass preset:

  • HSERDY = 0

  • PLL3RDY = 0

  • USBPHYC clock setup failed with HAL status 0x03

So I could not yet verify USBPHYC using the board HSE. The current working-but-failing path is still HSI -> PLL3Q -> USBPHYC 24 MHz, where the first EP0 SETUP fails with TXERR.

According to UM3276, the NUCLEO-H7S3L8 default HSE source should be the on-board 24 MHz X1 crystal. Is there any board revision, solder bridge, boot configuration, or power condition that would make HSERDY stay 0 on a default NUCLEO-H7S3L8?

Also, is HSI -> PLL3Q -> USBPHYC 24 MHz expected to be reliable enough for USB_OTG_HS embedded PHY host mode, or should HSE be considered mandatory in practice?

ST Technical Moderator
June 12, 2026

Hi ​@wooseong 

Would you attach minimum firmware to reproduce the issue?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
wooseongAuthor
Associate
June 15, 2026

Hi,

Thank you for your reply.

I prepared and attached a minimum firmware package to reproduce the issue.

The intended test flow is:

  1. bring up CN2 as USB Host/Source,

  2. enumerate and mount the USB MSC device,

  3. open INPUT.WAV from the USB stick,

  4. copy it byte-for-byte to OUTPUT.WAV.

The WAV file is not parsed or processed; it is only used as a normal test file. The purpose is to isolate the USB Host MSC / USBX / HCD / Type-C path from the original application.

A few notes for reproducing:

  • Board: NUCLEO-H7S3L8

  • STM32Cube_FW_H7RS_V1.3.0

  • XSPI2_HSLV=1 option byte is required

  • The official CDC_Standalone example enumerates correctly on CN2 as a USB serial device on my board

  • This minimum firmware uses HSE 24 MHz for USBPHYC

  • CN2 VBUS/source path is enabled through PM9/TCPP03

  • TCPP03 is detected on I2C3 at address 0x68

Current result:

  • HSERDY=1

  • USBPHYC HSE/24 MHz clock setup succeeds

  • TCPP03 source path setup succeeds

  • The USB root port detects the device connection and the port reset completes

  • USBX reports UX_DEVICE_CONNECTION

  • Enumeration then fails before VID/PID are read

  • The failure happens around the EP0 control transfer / SET_ADDRESS stage

  • HCD channel 0 ends with URB_ERROR, xfer_count=0

So the firmware currently does not reach the FileX mount or the actual INPUT.WAV copy step because USB enumeration fails first.

If ST already has a USB Host MSC example for the NUCLEO-H7S3L8 board, even a simple one that reads a file from a USB stick, I would be very grateful if you could share it or point me to it. I can then compare my initialization sequence against the official reference.

FBLBest answer
ST Technical Moderator
June 26, 2026

Hi ​@wooseong 

Apologies for the delayed response, and thank you for sharing the minimal firmware package.

This is very helpful. Can you confirm CDC_Standalone example in host mode is working as expected on the Nucleo H7S3?

I found two ST reference examples that may be useful as a baseline for the USB Host MSC path:

  • X-CUBE-AZRTOS-H7RS /Projects/STM32H7S78-DK/Applications/USBX/Ux_Host_MSC

  • STM32CubeH7RS /Projects/STM32H7S78-DK/Applications/USB_Host/MSC_RTOS

These examples are for STM32H7S78-DK, not NUCLEO-H7S3L8, but they should still help you compare the USB host, USBX, and MSC initialization sequence.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL