Skip to main content
Evan .1
Associate III
May 26, 2020 9:30 AM UTC
Question

NUCLEO-H7A3ZI-Q SPI_B LOW_LEVEL_DRIVER example

Hi,

I'm trying to get SPI_B on the NUCLEO-H7A3ZI-Q to work with low level drivers. But I have no output:

This is my code:

   LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);

   LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);

    /* SPI1 /CS */

    GPIO_InitStruct.Pin      = LL_GPIO_PIN_4;

    GPIO_InitStruct.Mode     = LL_GPIO_MODE_ALTERNATE;

    GPIO_InitStruct.Pull     = LL_GPIO_PULL_UP;

    GPIO_InitStruct.Speed    = LL_GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

    LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

    /* SPI1 SCK GPIO pin configuration*/

    GPIO_InitStruct.Pin      = LL_GPIO_PIN_3;

    GPIO_InitStruct.Mode     = LL_GPIO_MODE_ALTERNATE;

    GPIO_InitStruct.Pull     = LL_GPIO_PULL_DOWN;

    GPIO_InitStruct.Speed    = LL_GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

    LL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* SPI1 MISO GPIO pin configuration*/

    GPIO_InitStruct.Pin      = LL_GPIO_PIN_4;

    GPIO_InitStruct.Mode     = LL_GPIO_MODE_ALTERNATE;

    GPIO_InitStruct.Pull     = LL_GPIO_PULL_UP;

    GPIO_InitStruct.Speed    = LL_GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

    LL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* SPI1 MOSI GPIO pin configuration*/

    GPIO_InitStruct.Pin      = LL_GPIO_PIN_5;

    GPIO_InitStruct.Mode     = LL_GPIO_MODE_ALTERNATE;

    GPIO_InitStruct.Pull     = LL_GPIO_PULL_UP;

    GPIO_InitStruct.Speed    = LL_GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

    LL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   LL_SPI_InitTypeDef  SPI_InitStruct;

 /* Configure SPI MASTER ****************************************************/

 /* Enable SPI1 Clock */

 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);

 /* Configure the SPI1 parameters */

 SPI_InitStruct.BaudRate         = LL_SPI_BAUDRATEPRESCALER_DIV256;

 SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;

 SPI_InitStruct.ClockPhase       = LL_SPI_PHASE_2EDGE;

 SPI_InitStruct.ClockPolarity    = LL_SPI_POLARITY_LOW;

 SPI_InitStruct.BitOrder         = LL_SPI_MSB_FIRST;

 SPI_InitStruct.DataWidth        = LL_SPI_DATAWIDTH_8BIT;

 SPI_InitStruct.NSS              = LL_SPI_NSS_HARD_OUTPUT;

 SPI_InitStruct.CRCCalculation   = LL_SPI_CRCCALCULATION_DISABLE;

 SPI_InitStruct.Mode             = LL_SPI_MODE_MASTER;

 LL_SPI_Init(SPI1, &SPI_InitStruct);

 /* Lock GPIO for master to avoid glitches on the clock output */

 LL_SPI_EnableGPIOControl(SPI1);

 LL_SPI_EnableMasterRxAutoSuspend(SPI1);

 /* Set number of date to transmit */

 //LL_SPI_SetTransferSize(SPI1, 1);

 /* Enable SPI1 */

 LL_SPI_Enable(SPI1);

  while (1)

  {

     LL_SPI_TransmitData8(SPI1, 0x5A);

      while (LL_SPI_IsActiveFlag_RXP(SPI1) == 0);

  }

Sugestions what is wrong?

Thanks!.

This topic has been closed for replies.