Skip to main content
jkasper
Associate II
Apr 2, 2021 9:43 PM UTC
Solved

NUCLEO F413 User USB Connection

Hello!

I am connecting my nucleo to my computer through the user usb. I have set FDMOD and received the USBRST message and initialized the endpoint, but after i receive ENUMDNE I never receive the RXFLVL interrupt.

Here is the output of dmesg on my computer:

[ 6544.461644] usb 1-10: new full-speed USB device number 56 using xhci_hcd
[ 6544.589741] usb 1-10: device descriptor read/64, error -71
[ 6544.829707] usb 1-10: device descriptor read/64, error -71
[ 6545.065646] usb 1-10: new full-speed USB device number 57 using xhci_hcd
[ 6545.197659] usb 1-10: device descriptor read/64, error -71
[ 6545.433727] usb 1-10: device descriptor read/64, error -71
[ 6545.541712] usb usb1-port10: attempt power cycle
[ 6546.197666] usb 1-10: new full-speed USB device number 58 using xhci_hcd
[ 6546.197770] usb 1-10: Device not responding to setup address.
[ 6546.405772] usb 1-10: Device not responding to setup address.
[ 6546.613665] usb 1-10: device not accepting address 58, error -71
[ 6546.741727] usb 1-10: new full-speed USB device number 59 using xhci_hcd
[ 6546.741834] usb 1-10: Device not responding to setup address.
[ 6546.949770] usb 1-10: Device not responding to setup address.
[ 6547.157675] usb 1-10: device not accepting address 59, error -71
[ 6547.157753] usb usb1-port10: unable to enumerate USB device

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Apr 2, 2021 11:04 PM UTC

To exclude hardware problems: can the DFU bootloader enumerate?

The Synopsys OTG is very picky. Check clocks and FIFO settings (don't forget they are in words). Post relevant portions of code.

JW

7 replies

waclawek.jan
waclawek.janBest answer
Super User
Apr 2, 2021 11:04 PM UTC

To exclude hardware problems: can the DFU bootloader enumerate?

The Synopsys OTG is very picky. Check clocks and FIFO settings (don't forget they are in words). Post relevant portions of code.

JW

jkasper
jkasperAuthor
Associate II
Apr 6, 2021 12:10 AM UTC

Hi JW,

Yes, the dfu enumerates.

It looks like the 413 requires an HSE clock to use usb otg so i'm installing an external crystal. But then how does the dfu work?

waclawek.jan
Super User
Apr 6, 2021 7:10 AM UTC

STLink outputs an 8MHz clock, the target mcu can use it in HSE Bypass mode, if the appropriate jumpers/solder bridges are set. See the Nucleo's manual.

JW

jkasper
jkasperAuthor
Associate II
Apr 6, 2021 4:51 PM UTC

I'm just wondering how the dfu works without an hse. The stlink mco shouldn't be connected because the solder bridges aren't set as specified in the manual. If the dfu works, do i actually need an hse?

jkasper
jkasperAuthor
Associate II
Apr 6, 2021 6:58 PM UTC

Turns out my pllq config was off, didn't need to enable mco or add crystal!

waclawek.jan
Super User
Apr 6, 2021 7:26 PM UTC

The HSI may be good enough for a reasonably working USB device - at this temperature, in this piece of silicon, with this configuration of other on-chip and on-board resources - but that does not mean it's OK.

JW

jkasper
jkasperAuthor
Associate II
Apr 6, 2021 8:15 PM UTC

Yes i'll definitely add an x3 crystal, i just wanted to know if it was mandatory to enable hse to get an otg connection

Thanks for your help!