Skip to main content
Associate
Feb 20, 2025 6:31 AM UTC
Solved

Nucleo-F103rb Keyboard

I'm new to fiddling with MCUs, so I'm looking for some advice, I'm working on a project for my class and I'm trying to emulate a keyboard using the nucleo-F103rb. I have my code written out, I have a usb cable with D+ Connected to PA12 and D- to PA11, GND to GND and VCC to E5V all within CN5. Despite having all the headers in place, my computer doesn't detect any connection whatsoever. If anyone could suggest anything that may help it'd be really appreciated. 

This topic has been closed for replies.
Logan_Best answer
Associate
Feb 21, 2025 5:35 PM UTC

I have not, albeit I have looked at the ST videos based on "stm32 usb training", ill check this out too as well as trying with a 1.5 kOhm pullup and update this post when I do. Much appreciated.

11 replies

TDK
Feb 20, 2025 1:54 PM UTC

Do you have a 1.5 kOhm pullup on USB_DP?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Logan_Author
Associate
Feb 21, 2025 5:33 PM UTC

I currently do not, I'm a little new to this so excuse my lack of knowledge, would any 1.5 kOhm resistor from amazon or whatnot work fine?

TDK
Feb 21, 2025 5:46 PM UTC

Yes, any resistor should work.

The STM32F1 is very old. Newer families have an integrated pullup that is activated when the USB is used. I'd recommend switching to a newer family if you can.

Introduction to USB hardware and PCB guidelines using STM32 MCUs - Application note

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Feb 20, 2025 7:30 PM UTC

Hi @Logan_ 

I'd add another question apart the hardware check suggested by @TDK 

Have you tried the example provided for a mouse?

STM32CubeF1/Projects/STM32F103RB-Nucleo/Applications/USB_Device/HID_Standalone at master · STMicroelectronics/STM32CubeF1

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Logan_AuthorBest answer
Associate
Feb 21, 2025 5:35 PM UTC

I have not, albeit I have looked at the ST videos based on "stm32 usb training", ill check this out too as well as trying with a 1.5 kOhm pullup and update this post when I do. Much appreciated.