Skip to main content
Maksim Illarionov
Visitor II
Feb 21, 2018 9:51 AM UTC
Question

Notification SERIAL_STATE on VCP STM32F105

Posted on February 21, 2018 at 10:51

Hello everyone! I'm trying to send a SERIAL_STATE notification to the host.

The example was raised earlier

https://community.st.com/message/89959

.

When sending a buffer to CDK_CMD_EP, with USB_LL_Transmit the device stops responding. If I for example send a buffer to CD_OUT_EP or CDC_IN_EP, the data is sent and I can see them in the terminal.

Someone can already implemented the similar?

Thank you very much, waiting for your answers.

uint8_t CDC_Serial_State_Buf[10] = {
 0xA1, // vmRequestType
 0x09, // SERIAL_STATE
 0x00, // wValue
 0x00,
 0x00, // wIndex
 0x00,
 0x00, // wLength
 0x01,
 0x00, // UART state bitmap
 0x00,
 };
uint8_t CDC_Serial_State(void)
{
 USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0)
 {
 return USBD_BUSY;
 }
hUsbDeviceFS.ep0_state = USBD_EP0_STATUS_IN;
hUsbDeviceFS.ep_in[0].total_length = 10;
hUsbDeviceFS.ep_in[0].rem_length = 10;
 /* Start the transfer */
 USBD_LL_Transmit (&hUsbDeviceFS, CDC_CMD_EP, CDC_Serial_State_Buf, 10);
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 return USBD_OK;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#stm32f105 #vcp #serial_state #stm32-virtual-com-port #usb-cdc-serial_state
This topic has been closed for replies.