Skip to main content
Visitor II
Jun 18, 2025 4:14 PM UTC
Question

Normal USB CDC Cannot Define after update.

I was used normal mode USB CDC with Host Only -> and in middleware ( USB CDC) And it worked no matter what and good for beginners. After Update That files ware missed with same settings-up for new project. i was in middle in middle of the project for normal USB cdc. if STM programmers need to do that they have to it like new menu item and add new descriptor method or some what then users can understand and now we struck.. if some one updated his project i don't know what happened.. now i'm at middle cannot go forward.. 

This topic has been closed for replies.

1 reply

ST Technical Moderator
Oct 23, 2025 4:17 PM UTC

Hi @Laksahan 

Did you refer to examples firmware provided for F4 in host mode? If so, could you specify which example you are having difficulties with?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL