Skip to main content
FIser.1
Visitor II
Feb 16, 2021 9:18 PM UTC
Question

No connection in STM32CubeMonitor-UCPD (NUCLEO-G474RE + X-NUCLEO-USBPDM1)

Hey,

I followed the intructions of the Youtube video and put the code in the files like it is described in AN5418 for the STMG474RE.

There were no errors after building the code. So I flashed it to the board and tried to run this example.

But the STM32CubeMonitor does not show any connected board...

The only thing i can do is see the COM port in 'select tracer port'.

I read some other Questions about the same problem and tried to find a way to make it work but until now nothing changed.

Have i forgotten something or is it possibly the firmware version or something like that?

This topic has been closed for replies.

1 reply

Igor Cesko
ST Employee
Apr 14, 2021 3:41 PM UTC

Hi

This is a complex problem.

I suggest that you can run example provided in the STM32G4 Cube: download STM32Cube_FW_G4_V1.4.0 library and the USBPD application is located here:

"\Repository\STM32Cube_FW_G4_V1.4.0\Projects\B-G474E-DPOW1\Applications\USB-PD" 

Regards

Igor