Skip to main content
Associate
Nov 9, 2025 8:58 PM UTC
Solved

Newbie struggling with Complimentary Output of Timer

Hi,

first foray into STM32 with a Nucleo-F7222ZE.

Using CubeMX I have set up Timer1 to generate PWM. I can get outputs OC1, OC2, OC3 etc, but I cannot get the complementary outputs OC1N, OC2N, OC3N to operate.

 

I feel like I'm missing something, like dead band between OC1 and OC1N for example..

I've tried just about every combination I can think of in CubeMX, with no result so far.

 

Craig

TDK
TDKBest answer
Nov 9, 2025 10:02 PM UTC

The correct function to use to start a complementary channel is HAL_TIMEx_PWMN_Start. For example, to start channel TIM1_CH2N:

HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);

 

> HAL_TIM_PWMN_Start

> HAL_TIM1_PWMN_Start

Neither of these are functions that exist in HAL. Perhaps copy/paste to avoid typos.

"If you feel a post has answered your question, please click ""Accept as Solution""."

8 replies

TDK
Nov 9, 2025 9:06 PM UTC
"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Nov 9, 2025 9:11 PM UTC

Hi,

thanks for your reply, and I rather think you are on to it. I have used this:

HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_1);

 

to start the timer. Your reply suggests I need to start the complementary output specifically. I'll try it. 

Thanks

Craig

Associate
Nov 9, 2025 9:57 PM UTC

Hi, I have tried:

 

HAL_TIM_PWMN_Start(.....

HAL_TIM1_PWMN_Start(

 

and  get compile errors whenever I try to include either the timer number (1) or the  'N' for complementary

 

Craig