Skip to main content
MC.5
Associate
Oct 20, 2022 11:01 AM UTC
Solved

New Lib reentrant using C++ and RTOS

I am confused on the topic of new lib reentrant and RTOS.

I use C++ and do some std::make_unique calls so malloc it's probably getting called under the hood.

I have enabled the setting configUSE_NEWLIB_REENTRANT for RTOS and I am using heap_4 memory scheme.

I am using a single core microcontroller from the family STM32L4.

Is this enough to avoid problems ?

I got confused by the posts on this topic by "nadler" and "mcuoneclipse"

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Oct 20, 2022 4:51 PM UTC

> I got confused by the posts on this topic by "nadler" and "mcuoneclipse"

Welcome to the club :)

>  I am using heap_4 memory scheme.

All heap_N except of heap_3 are not aware of the C library heap (malloc/free/new...).

Either make all allocations from the C heap before starting the RTOS scheduler (and avoid calling malloc &free from tasks), or read on thread-safe implementation of malloc/free for newlib.

4 replies

Pavel A.
Pavel A.Best answer
Oct 20, 2022 4:51 PM UTC

> I got confused by the posts on this topic by "nadler" and "mcuoneclipse"

Welcome to the club :)

>  I am using heap_4 memory scheme.

All heap_N except of heap_3 are not aware of the C library heap (malloc/free/new...).

Either make all allocations from the C heap before starting the RTOS scheduler (and avoid calling malloc &free from tasks), or read on thread-safe implementation of malloc/free for newlib.

MC.5
MC.5Author
Associate
Oct 24, 2022 9:19 AM UTC

Hi Pavel,

thank you a lot for the reply.

The codebase that I am working on makes all the objects allocations before starting freeRTOS. So I think that I am safe.

Do you think that I can avoid using the setting configUSE_NEWLIB_REENTRANT if I don't do dynamic allocation and I don't use the regular snprintf ?

Thank you again.

Kind regards,

Mattia

Pavel A.
Oct 24, 2022 1:06 PM UTC

Hi Mattia

Newlib has some other functions that use the per-thread area (I don't remember which exactly). Likely yes, if the program does not use any of these in several threads, it can get away without configUSE_NEWLIB_REENTRANT.