Skip to main content
Associate III
Nov 21, 2024 7:48 PM UTC
Solved

NetX Duo with STM32H5xx

Hello, 

On the ST wiki for NetX Duo [ Introduction to NETXDUO - stm32mcu ], there is the following info tag:

potatobandit_0-1732217910178.png

"Information - NetX requires that Zero-copy feature that is currently supported only in the STM32H7 HAL Ethernet driver. "

I have run the NetXDuo example application on the STM32H563ZI eval board and it's functioning as expected. I'm trying to understand what the limitation is for running NetX Duo on the H5 vs the H7, as this comment implies that I have to upgrade to the H7 to use the feature all together. 

If I choose to run NetX Duo on the H5, is there a subset of features that won't work? Is zero-copy just not available? 

 

Thanks

This topic has been closed for replies.
STeaBest answer
ST Employee
Nov 21, 2024 10:24 PM UTC

Hello @potatobandit ,

There is no limitation when using NetXDuo with STM32H5 series. this note and article came before the H5 series introduction and needs to be updated thank you for pointing this out.

You can get more examples using the hole azure ecosystem on STM32H5 in STM32CubeH5 - STM32Cube MCU Package for STM32H5 series (HAL, Low-Layer APIs and CMSIS, USB, TCP/IP, File system, RTOS, Graphic - and examples running on ST boards) - STMicroelectronics


Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STeaBest answer
ST Employee
Nov 21, 2024 10:24 PM UTC

Hello @potatobandit ,

There is no limitation when using NetXDuo with STM32H5 series. this note and article came before the H5 series introduction and needs to be updated thank you for pointing this out.

You can get more examples using the hole azure ecosystem on STM32H5 in STM32CubeH5 - STM32Cube MCU Package for STM32H5 series (HAL, Low-Layer APIs and CMSIS, USB, TCP/IP, File system, RTOS, Graphic - and examples running on ST boards) - STMicroelectronics


Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Nov 21, 2024 11:46 PM UTC

Thank you!