Skip to main content
Bilge
Associate III
Dec 5, 2018 8:29 AM UTC
Question

Need help to run Ethernet communication correctly with STM32H7 nucleo?

 Is there anybody who can ran ethernet communication correctly with stm32h7 nucleo?

This topic has been closed for replies.

43 replies

Jack3
Senior
Feb 12, 2019 10:21 AM UTC

Hi @Bilge​ ,

I think this is missing before the main loop:

 /* Http webserver Init */

 udp_echoserver_init();

Did you get it working?

Regards,

Jack.

Bilge
BilgeAuthor
Associate III
Jun 20, 2019 11:41 AM UTC

Hi @Jack​  ,

I can ping to my board without packet losses. My current goal is to send and receive packets with udp protocol.

Regards,

Bilge.

CodesMagic
Associate II
Jun 10, 2019 8:31 AM UTC

Hi dear Imen,

I'm using STM32Cube_FW_H7_V1.4.0 and still I'm not able to ping my board.

I've disabled DHCP, and I'm not using RTOS.

Most of the settings were left at their defaults. However, to enable the webserver, the following

options were enabled: LWIP_HTTPD, LWIP_HTTPD_CGI and LWIP_HTTPD_SSI. Because the Nucleo

board has bucket loads of memory, the maximum tag length (LWIP_HTTPD_MAX_TAG_NAME_LEN)

was increased from 8 to 16 characters.

May I ask you to help me by providing step by step instruction?

CodesMagic
Associate II
Jun 10, 2019 1:39 PM UTC

I've attached my project.

Please let me know how can I solve my problem.

Thank you in advance.

:loudly_crying_face:

Bilge
BilgeAuthor
Associate III
Jun 25, 2019 6:41 AM UTC
  • Hi,@Imen DAHMEN​ 
  • I don't ask new question on the st community web page .I get an error message " You can't add new topics, so select existing topics for your post " .

ST Technical Moderator
Jun 25, 2019 9:41 AM UTC

Hi @Bilge​ ,

Community members are not able to create new topics ( topic = tag). Only ST employees and moderators can do that.

If you want to add/edit your Topic, you should use the existing one.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NKarn.1
Associate II
Feb 12, 2020 2:44 PM UTC

Hi All,

Just to recieve an update on the firmware bug for ethernet. Is it fixed ? I am trying to ping ethernet to PC but not able to send any packets in NucleoH743ZI board.

alister
Senior III
Feb 12, 2020 10:07 PM UTC

My fixes and improvements to ST's STM32H7 ETH driver and lwIP ethernetif.c are at https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet.

Source code and documentation attached.

I don't use evaluation boards or build example code.

You'll have to port my changes yourself.