Skip to main content
tgrant
Associate II
November 27, 2019
Question

Need help getting SD+FATFS working with an STM32H747I-Disco

  • November 27, 2019
  • 7 replies
  • 2841 views

I'm trying to use the SD card reader on the STM32H747I-Disco with FatFs. It's working as expected with the M7 core -- I'm able to initialize the SD interface and the filesystem, and access files on the SD card.

However, when I perform the same initialization using the M4 core (which is the core I would like to access the SD card), I get FR_DISK_ERROR when I try to open files or directories.

I'm using the BSP initialization functions. The SD interface initializes correctly (without error, anyway), and BSP_SD_GetCardInfo returns the correct information. After I link the driver, I'm able to mount the SD card, but attempting to open a file fails.

The failing part of my setup code looks something like this:

 if( FATFS_LinkDriver( &SD_Driver, sdPath ) != 0 )
 {
 sendString( "FATFS error: unable to link driver!\r\n" );
 }
 else if( (res = f_mount( &sdFatFs, (TCHAR const*)sdPath, 0 )) != FR_OK )
 {
 sendString( "FATFS error: unable to mount SD card!\r\n" );
 }
 else if( (res = f_open( &file, "test.txt", FA_READ )) != FR_OK )
 {
 // This call fails with FR_DISK_ERROR
 sendString( "FATFS error: unable to open file!\r\n" );
 }

Does anybody know why FatFs would work on one core and not the other? Is anyone successfully using the SD interface with the M4 core?

This topic has been closed for replies.

7 replies

tgrant
tgrantAuthor
Associate II
November 28, 2019

I have found a solution.

The M7 is being clocked at 400MHz, and the M4 is at 200MHz. I noticed that doubling the clock divider set in BSP_SD_Init caused the file operations to start working on the M4. I wasn't too keen on modifying that function, so instead I found the clock source for SDMMC1 (PLL1) and set the divider to supply a 200MHz clock to the SDMMC.

It's not clear to me what the relationship between the different clocks is, but I'm happy to have it working for now.

TurtleBeach
Associate II
December 9, 2019

@tgrant,

Would you be willing to share a few more details/guidance related to how you managed to get an SD Card / FatFS working on the DISCO board?

I have been struggling for the past 3 days, to no avail. I am using CubeIDE 1.1, with CubeMX 5.4. Since there is no direct H747-DISCO SD Card project/example, I have been attempting to modify the H747-EVAL example for FatFS. I actually want to access the SD Card from the M7 processor, but the SD Card is not getting initialized. I have tried to faithfully follow the rat's nest of #defines and #includes to get the proper BSP_SD_Init code, but I don't think I have it, and I also think the problem is related to clock speeds. In my case, I **think** the right clocks are being initialized in the SystemClock_Config() that I pulled from the -EVAL application, but I am frankly not sure (I expect to eventually figure out what I need to know about the clocks and configuration, but right now I just need working code that will let me pull a couple of files off an SD Card). I did not expect this to be the nightmare it has become.

Thanks.

Tesla DeLorean
Guru
December 9, 2019

>>Since there is no direct H747-DISCO SD Card project/example...

STM32Cube_FW_H7_V1.5.0\Projects\STM32H747I-DISCO\Examples\JPEG\JPEG_DecodingUsingFs_DMA

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LBarn.1
Associate II
February 11, 2020

This seems very similar to the issue I posted in December. Would the stack and heap size have any affect on this? Where are they stored in the Cube IDE project?

Thanks in advance for your reply.

Tesla DeLorean
Guru
February 11, 2020

For CubeIDE (GNU/GCC) the stack/heap generally commingled, and are called out in the linker script. The actually allocator code is actually in the __sbrk() code in newlibs.c or syscalls.c

Generally you want the stack in the fastest available memory (DTCM SRAM)

The H7 has some particularly difficult memory/dma controller issues, so one must pay attention to memory alignment, and cache coherency.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..