Skip to main content
Associate II
Oct 15, 2024 7:30 AM UTC
Question

Mutliple TCP clients on STM32H563 with NetXDuo

I have a question regarding the tutorial "Handling multiple TCP clients on STM32H563 with NetX Duo" written by @STea .

See https://community.st.com/t5/stm32-mcus/handling-multiple-tcp-clients-on-stm32h563-with-netx-duo/ta-p/695030

 

In the first section "handling multilple clients on the same port", there is some example code. In the function

static VOID tcp_thread_entry(ULONG thread_input)

there is an infinite loop, containing a tx_queue_receive call:

 /* Receive pointers to TCP socket and network packet from TCP callback */
 ULONG msg[2];
 status = tx_queue_receive(&g_tcp_q, msg, TX_WAIT_FOREVER);

At the moment I try to create an application based on this tutorial. Apparently, the tx_queue_receive fails (returns TX_QUEUE_ERROR) which makes sense, since no one sends data into the queue "g_tcp_q". At which point should this happen? I can't find it in the example code.

 

Furthermore, the tutorial states "You can find attached the file app_netxduo++clients_same_port.c that you can replace in this project to test this use case.". I can't find it.

 

This topic has been closed for replies.

2 replies

ST Employee
Oct 15, 2024 8:05 AM UTC

Hello @SiSte ,

the queue receives message from the receive callback 
here is the section where it gets messages published to thread app 

static void g_tcp_sck_receive_cb(NX_TCP_SOCKET * p_sck)
{
 NX_PACKET * p_packet;

 /* This callback is invoked when data is already received. Retrieving
 * packet with no suspension. */
 nx_tcp_socket_receive(p_sck, &p_packet, NX_NO_WAIT);

#if APP_TCP_LOG
 ULONG ip, client_port;
 nx_tcp_socket_peer_info_get(p_sck, &ip, &client_port);
 printf("[TCP %x] Incoming packet (%lu bytes) from %lu.%lu.%lu.%lu:%lu\n\r",
 p_sck, p_packet->nx_packet_length, (ip >> 24) & 0xFF,
 (ip >> 16) & 0xFF, (ip >> 8) & 0xFF, (ip) & 0xFF, client_port);
#endif

#if APP_TCP_INSTANT_ECHO
 /* Send packet back on the same TCP socket */
 nx_tcp_socket_send(p_sck, p_packet, NX_NO_WAIT);
#else
 ULONG msg[2] =
 {
 (ULONG) p_sck, (ULONG) p_packet
 };

 /* Sent TCP socket and packet pointers to user thread */
 if (TX_SUCCESS != tx_queue_send(&g_tcp_q, msg, TX_NO_WAIT))
 {
 nx_packet_release(p_packet);
 }
#endif
}

 and you are right the attached are missing from the article sorry for the inconvenience and here is the file attached.

Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SiSteAuthor
Associate II
Oct 15, 2024 8:45 AM UTC

Thanks for your fast reply. Regarding the TX_QUEUE g_tcp_q:

As far as I understand ThreadX, it is required to call "tx_queue_create()" before calling send or receive on the queue.

I can't see this call in our code, might this be the reason for getting a TX_QUEUE_ERROR returned from tx_queue_receive()?