Skip to main content
Visitor II
Jul 30, 2024 6:55 PM UTC
Question

Multiple HID reports is

Hi All, 

I'm having issues setting up multiple HID reports. 
I had a couple of USB HID projects in the past, all worked fine. This time I started from STM32CubeIDE from Custom HID device. 

I have the following report descriptor:

 

 

/** Usb HID report descriptor. */
__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =
{
 /* USER CODE BEGIN 0 */
		
		0x05, 0x01, // USAGE_PAGE (Generic Desktop)
		0x09, 0x04, // USAGE (Joystick)
		0xa1, 0x01, // COLLECTION (Application)

		0x85, 3,			 		 // REPORT_ID

		0x05, 0x09, // USAGE_PAGE (Button)
		0x19, 0x01, // USAGE_MINIMUM (Button 1)
		0x29, 0x25, // USAGE_MAXIMUM (Button 37)
		0x25, 0x01, // LOGICAL_MAXIMUM (1)
		0x15, 0x00, // LOGICAL_MINIMUM (0)
		0x75, 0x01, // REPORT_SIZE (1)
		0x95, 0x25, // REPORT_COUNT (37)
		0x65, 0x00,					 // UNIT (None)
		0x81, 0x02, // INPUT (Data,Var,Abs)
		0x75, 0x01,			 		 // REPORT_SIZE (1)
		0x95, 0x03, 		 	 // REPORT_COUNT (# of padding bits)
		0x81, 0x03, 	 	 // INPUT (Const,Var,Abs)

		0x05, 0x01, // USAGE_PAGE (Generic Desktop)
		0x09, 0x33, // USAGE (RX)
		0x09, 0x34, // USAGE (RY)
		0x15, 0x00, // LOGICAL_MINIMUM (0)
		0x26, 0xA0, 0x0f, // LOGICAL_MAXIMUM (4000)
		0x75, 0x10, // REPORT_SIZE (16)
		0x95, 0x02, // REPORT_COUNT (2)
		0x81, 0x02, // INPUT (Data,Var,Abs)

		0xC0, 						 // End collection

		0x06, 0x00, 0xff, 		 // Usage Page (Vendor Defined)
		0x09, 0x01, 		 // Usage (Vendor Usage 1)
		0xa1, 0x01, 		 // Collection (Application)
									 
		0x85, 90,			 		 // REPORT_ID
									 
		0x15, 0x00, 		 // LOGICAL_MINIMUM (0)
		0x26, 0xff, 0x00, 		 // LOGICAL_MAXIMUM (1)
		0x75, 0x08, 		 // Report Size (8)
									 
		0x95, 19, 		 // Report Count (32)
		0x91, 0x02, 		 // Output (Data,Var,Abs)
									 
		0x95, 19, 		 // Report Count (32)
		0x81, 0x02, 		 // Input (Data,Var,Abs)


 /* USER CODE END 0 */
 0xC0 /* END_COLLECTION	 */
};

 

 

 So, a game controller + 32 byete IN/OUT for communication.

  1. Everything works fine when testing the parts separately (only game controller section or only custom message IN/OUT section
  2. It also works if I delete the message input part 
    0x95, 19,                 // Report Count (32)
    0x81, 0x02,               // Input (Data,Var,Abs)
  3. But as soon as I have the input part also, the reports are not properly sent/received 
  4. However, if I start reporting with 33 bytes (report ID +32) for the game controller part, it works again.

So, the custom input report somehow affects the game controller reports. It doesn't matter what I set for report count in the custom report, it works only if the game controller has the same size. In USB monitor it looks like only 32 byte messages are received and if I report smaller ones, then it waits until it's full. (But I'm not sure that this is on PC side or mcu.) 

 

 

HAL_Delay(2000);
// Game controller report
uint8_t data[33] = {3};
USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, data, 33);
HAL_Delay(2000);
// Customer report
uint8_t data2[33] = {90};
USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, data2, 33);

 

 

So the lines above work fine, but the game controller report should be 9 byte + reportID, instead of 33.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Aug 12, 2024 6:17 PM UTC

Hi @PDan 

Which product are you using? HID report descriptor might not correctly define the different report sizes

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL