Skip to main content
Associate
Oct 26, 2023 2:26 PM UTC
Question

Multiple ADC Channels (using registers)

Hello all, I am currently working on a project in which I need to sample 5 ADC channels every 50 ms. As of now, I am trying to use TIM2's TRGO (interrupt triggered every 50 ms) to trigger the conversion of a regular sequence of 5 ADC channels (PA0 - PA4) and save these values by reading the ADC's data register in the ADC IRQ (triggered by the EOC interrupt flag). For some reason, I cannot figure out why the EOC interrupt is only triggered once, at the beginning of the program. If anyone could help, I would greatly appreciate it. 

 

I will post my code if needed (I am using the Keil uVision 5 IDE). Thanks in advance.

This topic has been closed for replies.

2 replies

Stassen.C
ST Employee
Oct 26, 2023 2:40 PM UTC

Hello Caden013, 

Could you please show us your code so that we can look at it?

Regards,
Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
caden013Author
Associate
Oct 26, 2023 2:42 PM UTC


@Stassen.C wrote:

Hello Caden013, 

Could you please show us your code so that we can look at it?

Regards,
Stassen


Yes, I will attach the ADC and Timer c files where I set their settings.

 

Here is where I setup their corresponding clocks (in a different file):

 

/*
FUNCTION: clockSetup
INPUTS: none
OUTPUTS: none
PURPOSE: To initialize the clocks for the peripherals
*/
void clockSetup(void)
{
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; // enable GPIOA clock
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; // enable GPIOB clock
RCC->AHB2ENR |= RCC_AHB2ENR_ADCEN; // enable ADC clock
RCC->APB1ENR1 |= RCC_APB1ENR1_TIM2EN; // enable clock for TIM2
}