Skip to main content
Visitor II
Apr 23, 2024 8:59 AM UTC
Question

mtp without threadx

Hello,

I want to use the USBX MTP stack on a stm32u5 without threadx. The configuration in stm32CubeMx worked fine but when i run the programm, i get UX_FUNCTION_NOT_SUPPORTED from this location:

 

UINT _ux_device_class_pima_initialize(UX_SLAVE_CLASS_COMMAND *command)
{
#if defined(UX_DEVICE_STANDALONE)
 UX_PARAMETER_NOT_USED(command);
 return(UX_FUNCTION_NOT_SUPPORTED);
#else
UINT status;
UX_SLAVE_CLASS_PIMA *pima;
UX_SLAVE_CLASS_PIMA_PARAMETER *pima_parameter;
UX_SLAVE_CLASS *class_ptr;

 

 Are there any other options to use the USBX MTP stack in standalone mode at the moment or are there any plans to support the standalone mode in the future?

Thanks in advance.

This topic has been closed for replies.

2 replies

ABOUA
ST Employee
May 2, 2024 3:37 PM UTC

Hello Codgen,

Only RTOS mode is supported for USBX device pima class driver

Regards,

Tesla DeLorean
Guru
May 2, 2024 3:44 PM UTC

There are perhaps third-party commercial libraries or you could DIY

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..