Skip to main content
TG.3
Associate II
Aug 25, 2022 6:37 AM UTC
Question

MQTT: authentication error in server side

Hi, I am new to MQTT and LWIP.

I am trying to implement MQTT client in STM32F407 and to connect to MQTT server through LWIP.

When I tried connecting to MQTT server, I received authentication error in server side.

Kindly help resolve the issue.

 

mqtt_client_connect(mqtt_client_t *client, const ip_addr_t *ip_addr, u16_t port, mqtt_connection_cb_t cb, void *arg,

          const struct mqtt_connect_client_info_t *client_info)

{

 err_t err;

 size_t len;

 u16_t client_id_length;

 /* Length is the sum of 2+"MQTT", protocol level, flags and keep alive */

 u16_t remaining_length = 2 + 4 + 1 + 1 + 2;

 u8_t flags = 0, will_topic_len = 0, will_msg_len = 0;

 

 LWIP_ASSERT("mqtt_client_connect: client != NULL", client != NULL);

 LWIP_ASSERT("mqtt_client_connect: ip_addr != NULL", ip_addr != NULL);

 LWIP_ASSERT("mqtt_client_connect: client_info != NULL", client_info != NULL);

 LWIP_ASSERT("mqtt_client_connect: client_info->client_id != NULL", client_info->client_id != NULL);

 

 if (client->conn_state != TCP_DISCONNECTED) {

  LWIP_DEBUGF(MQTT_DEBUG_WARN,("mqtt_client_connect: Already connected\n"));

  return ERR_ISCONN;

 }

 

 /* Wipe clean */

 memset(client, 0, sizeof(mqtt_client_t));

 client->connect_arg = arg;

 client->connect_cb = cb;

 client->keep_alive = client_info->keep_alive;

 mqtt_init_requests(client->req_list);

 

 /* Build connect message */

 if (client_info->will_topic != NULL && client_info->will_msg != NULL) {

  flags |= MQTT_CONNECT_FLAG_WILL;

  flags |= (client_info->will_qos & 3) << 3;

  if (client_info->will_retain) {

   flags |= MQTT_CONNECT_FLAG_WILL_RETAIN;

  }

  len = strlen(client_info->will_topic);

  LWIP_ERROR("mqtt_client_connect: client_info->will_topic length overflow", len <= 0xFF, return ERR_VAL);

  LWIP_ERROR("mqtt_client_connect: client_info->will_topic length must be > 0", len > 0, return ERR_VAL);

  will_topic_len = (u8_t)len;

  len = strlen(client_info->will_msg);

  LWIP_ERROR("mqtt_client_connect: client_info->will_msg length overflow", len <= 0xFF, return ERR_VAL);

  will_msg_len = (u8_t)len;

  len = remaining_length + 2 + will_topic_len + 2 + will_msg_len;

  LWIP_ERROR("mqtt_client_connect: remaining_length overflow", len <= 0xFFFF, return ERR_VAL);

  remaining_length = (u16_t)len;

 }

 

 /* Don't complicate things, always connect using clean session */

 flags |= MQTT_CONNECT_FLAG_CLEAN_SESSION;

 

 len = strlen(client_info->client_id);

 LWIP_ERROR("mqtt_client_connect: client_info->client_id length overflow", len <= 0xFFFF, return ERR_VAL);

 client_id_length = (u16_t)len;

 len = remaining_length + 2 + client_id_length;

 LWIP_ERROR("mqtt_client_connect: remaining_length overflow", len <= 0xFFFF, return ERR_VAL);

 remaining_length = (u16_t)len;

 

 if (mqtt_output_check_space(&client->output, remaining_length) == 0) {

  return ERR_MEM;

 }

 

 client->conn = tcp_new();

 if (client->conn == NULL) {

  return ERR_MEM;

 }

 

 /* Set arg pointer for callbacks */

 tcp_arg(client->conn, client);

 /* Any local address, pick random local port number */

 err = tcp_bind(client->conn, IP_ADDR_ANY, 0);

 if (err != ERR_OK) {

  LWIP_DEBUGF(MQTT_DEBUG_WARN,("mqtt_client_connect: Error binding to local ip/port, %d\n", err));

  goto tcp_fail;

 }

 LWIP_DEBUGF(MQTT_DEBUG_TRACE,("mqtt_client_connect: Connecting to host: %s at port:%"U16_F"\n", ipaddr_ntoa(ip_addr), port));

 

 /* Connect to server */

 err = tcp_connect(client->conn, ip_addr, port, mqtt_tcp_connect_cb);

 if (err != ERR_OK) {

  LWIP_DEBUGF(MQTT_DEBUG_TRACE,("mqtt_client_connect: Error connecting to remote ip/port, %d\n", err));

  goto tcp_fail;

 }

 /* Set error callback */

 tcp_err(client->conn, mqtt_tcp_err_cb);

 client->conn_state = TCP_CONNECTING;

 

 /* Append fixed header */

 mqtt_output_append_fixed_header(&client->output, MQTT_MSG_TYPE_CONNECT, 0, 0, 0, remaining_length);

 /* Append Protocol string */

 mqtt_output_append_string(&client->output, "MQTT", 4);

 /* Append Protocol level */

 mqtt_output_append_u8(&client->output, 4);

 /* Append connect flags */

 mqtt_output_append_u8(&client->output, flags);

 /* Append keep-alive */

 mqtt_output_append_u16(&client->output, client_info->keep_alive);

 /* Append client id */

 mqtt_output_append_string(&client->output, client_info->client_id, client_id_length);

 /* Append will message if used */

 if ((flags & MQTT_CONNECT_FLAG_WILL) != 0) {

  mqtt_output_append_string(&client->output, client_info->will_topic, will_topic_len);

  mqtt_output_append_string(&client->output, client_info->will_msg, will_msg_len);

 }

 return ERR_OK;

 

tcp_fail:

 tcp_abort(client->conn);

 client->conn = NULL;

 return err;

}

 

 

err_t

mqtt_publish(mqtt_client_t *client,const char *topic, const void *payload, uint16_t payload_length, u8_t qos, u8_t retain,

       mqtt_request_cb_t cb, void *arg)

{

 struct mqtt_request_t *r;

 u16_t pkt_id;

 size_t topic_strlen;

 size_t total_len;

 u16_t topic_len;

 u16_t remaining_length;

 LWIP_ASSERT("mqtt_publish: client != NULL", client);

 LWIP_ASSERT("mqtt_publish: topic != NULL", topic);

 LWIP_ERROR("mqtt_publish: TCP disconnected", (client->conn_state != TCP_DISCONNECTED), return ERR_CONN);

 

 topic_strlen = strlen(topic);

 LWIP_ERROR("mqtt_publish: topic length overflow", (topic_strlen <= (0xFFFF - 2)), return ERR_ARG);

 topic_len = (u16_t)topic_strlen;

 total_len = 2 + topic_len + payload_length;

 LWIP_ERROR("mqtt_publish: total length overflow", (total_len <= 0xFFFF), return ERR_ARG);

 remaining_length = (u16_t)total_len;

 

 LWIP_DEBUGF(MQTT_DEBUG_TRACE,("mqtt_publish: Publish with payload length %d to topic \"%s\"\n", payload_length, topic));

 

 if (qos > 0) {

  remaining_length += 2;

  /* Generate pkt_id id for QoS1 and 2 */

  pkt_id = msg_generate_packet_id(client);

 } else {

  /* Use reserved value pkt_id 0 for QoS 0 in request handle */

  pkt_id = 0;

 }

 

 r = mqtt_create_request(client->req_list, pkt_id, cb, arg);

 if (r == NULL) {

  return ERR_MEM;

 }

 

 if (mqtt_output_check_space(&client->output, remaining_length) == 0) {

  mqtt_delete_request(r);

  return ERR_MEM;

 }

 /* Append fixed header */

 mqtt_output_append_fixed_header(&client->output, MQTT_MSG_TYPE_PUBLISH, 0, qos, retain, remaining_length);

 

 /* Append Topic */

 mqtt_output_append_string(&client->output, topic, topic_len);

 

 /* Append packet if for QoS 1 and 2*/

 if (qos > 0) {

  mqtt_output_append_u16(&client->output, pkt_id);

 }

 

 /* Append optional publish payload */

 if ((payload != NULL) && (payload_length > 0)) {

  mqtt_output_append_buf(&client->output, payload, payload_length);

 }

 

 mqtt_append_request(&client->pend_req_queue, r);

 mqtt_output_send(&client->output, client->conn);

 return ERR_OK;

}

 

This topic has been closed for replies.

1 reply

MSG_ST
ST Employee
Oct 26, 2022 1:50 PM UTC

Hi,

There's an MQTT application example working on STM32F429ZI-Nucleo based on NetXDuo available here and which could help :

https://github.com/STMicroelectronics/x-cube-azrtos-f4/tree/main/Projects/STM32F429ZI-Nucleo/Applications/NetXDuo/Nx_MQTT_Client

Regards

Mahdy