Skip to main content
NKhad.1
Associate
Oct 4, 2021 12:04 AM UTC
Question

mongodb certification not inserted properly

On a choisi X-CUBE-CLD-GEN pour connecter la carte avec mongodb via mosquitt

Après le flash de la carte par le fichier bin et la configuration du wifi par le terminal(tera

term), l’insertion de la certification du mongodb n’a pas marché.

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
Oct 4, 2021 1:53 PM UTC

Hi @NKhad.1​ ,

In order to have more chance to get an answer, I am translating your post to English (commonly used language for our Community):

We chose X-CUBE-CLD-GEN to connect the board with mongodb via mosquitto. After downloading the bin file to the board and the configuration of the wifi by the terminal (teraterm), the inclusion of mongodb certification did not work.

Here I assume you are using B-L475E-IOT01 (based on your other question).

I also add relevant topic so that our experts can review this question.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Guillaume K
ST Employee
Oct 12, 2021 12:36 PM UTC

Hello

What do you mean by "l’insertion de la certification du mongodb n’a pas marché" / "The inclusion of mongodb certification did not work" ? could you give more details ?