Skip to main content
ABatt.1
Associate III
April 11, 2021
Solved

Modify usbd_stoge_if.c to use SD Card trougth SPI

  • April 11, 2021
  • 5 replies
  • 3655 views

Hi to all,

I managed to interface with the SD card through the SPI and the FaTFS library (thanks to https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/) now I need to implement a USB mass storage device on the same hardware.

i don't know how to modify usbd_stoge_if.c tin odero implement the functions:

int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size)

int8_t STORAGE_IsReady_FS(uint8_t lun)

Have you any suggestions?

Thanks.

This topic has been closed for replies.
Best answer by ABatt.1

At the end I was succerfully writed the file.

Here is my usbd_stoge_if.c, writed based on user_diskio_spi.c an user_diskio_spi.h from https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : usbd_storage_if.c
 * @version : v1.0_Cube
 * @brief : Memory management layer.
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under Ultimate Liberty license
 * SLA0044, the "License"; You may not use this file except in compliance with
 * the License. You may obtain a copy of the License at:
 * www.st.com/SLA0044
 *
 ******************************************************************************
 */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "usbd_storage_if.h"
#include "C:\ST\Progetti\Test_USB_2\STM32CubeIDE\Application\User\FATFS\Target\user_diskio_spi.h"
 
/* USER CODE BEGIN INCLUDE */
 
/* USER CODE END INCLUDE */
 
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE END PV */
 
/** @addtogroup STM32_USB_OTG_DEVICE_LIBRARY
 * @brief Usb device.
 * @{
 */
 
/** @defgroup USBD_STORAGE
 * @brief Usb mass storage device module
 * @{
 */
 
/** @defgroup USBD_STORAGE_Private_TypesDefinitions
 * @brief Private types.
 * @{
 */
 
/* USER CODE BEGIN PRIVATE_TYPES */
 
/* USER CODE END PRIVATE_TYPES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Defines
 * @brief Private defines.
 * @{
 */
 
#define STORAGE_LUN_NBR 1
//#define STORAGE_BLK_NBR 0x10000
#define STORAGE_BLK_NBR 0x3AB780
#define STORAGE_BLK_SIZ 0x200
 
/* USER CODE BEGIN PRIVATE_DEFINES */
 
/* USER CODE END PRIVATE_DEFINES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Macros
 * @brief Private macros.
 * @{
 */
 
/* USER CODE BEGIN PRIVATE_MACRO */
 
/* USER CODE END PRIVATE_MACRO */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Variables
 * @brief Private variables.
 * @{
 */
 
/* USER CODE BEGIN INQUIRY_DATA_FS */
/** USB Mass storage Standard Inquiry Data. */
const int8_t STORAGE_Inquirydata_FS[] = {/* 36 */
 
 /* LUN 0 */
 0x00,
 0x80,
 0x02,
 0x02,
 (STANDARD_INQUIRY_DATA_LEN - 5),
 0x00,
 0x00,
 0x00,
 'S', 'T', 'M', ' ', ' ', ' ', ' ', ' ', /* Manufacturer : 8 bytes */
 'P', 'r', 'o', 'd', 'u', 'c', 't', ' ', /* Product : 16 Bytes */
 ' ', ' ', ' ', ' ', ' ', ' ', ' ', ' ',
 '0', '.', '0' ,'1' /* Version : 4 Bytes */
};
/* USER CODE END INQUIRY_DATA_FS */
 
/* USER CODE BEGIN PRIVATE_VARIABLES */
 
/* USER CODE END PRIVATE_VARIABLES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Exported_Variables
 * @brief Public variables.
 * @{
 */
 
extern USBD_HandleTypeDef hUsbDeviceFS;
 
/* USER CODE BEGIN EXPORTED_VARIABLES */
 
/* USER CODE END EXPORTED_VARIABLES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_FunctionPrototypes
 * @brief Private functions declaration.
 * @{
 */
 
static int8_t STORAGE_Init_FS(uint8_t lun);
static int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size);
static int8_t STORAGE_IsReady_FS(uint8_t lun);
static int8_t STORAGE_IsWriteProtected_FS(uint8_t lun);
static int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);
static int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);
static int8_t STORAGE_GetMaxLun_FS(void);
 
/* USER CODE BEGIN PRIVATE_FUNCTIONS_DECLARATION */
 
/* USER CODE END PRIVATE_FUNCTIONS_DECLARATION */
 
/**
 * @}
 */
 
USBD_StorageTypeDef USBD_Storage_Interface_fops_FS =
{
 STORAGE_Init_FS,
 STORAGE_GetCapacity_FS,
 STORAGE_IsReady_FS,
 STORAGE_IsWriteProtected_FS,
 STORAGE_Read_FS,
 STORAGE_Write_FS,
 STORAGE_GetMaxLun_FS,
 (int8_t *)STORAGE_Inquirydata_FS
};
 
/* Private functions ---------------------------------------------------------*/
/**
 * @brief Initializes over USB FS IP
 * @param lun:
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Init_FS(uint8_t lun)
{
 /* USER CODE BEGIN 2 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 	 if(USER_SPI_initialize(0) == 0){
	 ret = USBD_OK;
 }
 
 return ret;//(USBD_OK);
 /* USER CODE END 2 */
}
 
/**
 * @brief .
 * @param lun: .
 * @param block_num: .
 * @param block_size: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size)
{
 /* USER CODE BEGIN 3 */
 //****** TO_DO *********
 *block_num = STORAGE_BLK_NBR;
 *block_size = STORAGE_BLK_SIZ;
 return (USBD_OK);
 /* USER CODE END 3 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_IsReady_FS(uint8_t lun)
{
 /* USER CODE BEGIN 4 */
	 USBD_StatusTypeDef ret = USBD_FAIL;
	 if(USER_SPI_status(0) == 0){
		 ret = USBD_OK;
	 }
	 return ret;
 return (USBD_OK);
 /* USER CODE END 4 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_IsWriteProtected_FS(uint8_t lun)
{
 /* USER CODE BEGIN 5 */
 return (USBD_OK);
 /* USER CODE END 5 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
 /* USER CODE BEGIN 6 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 if(USER_SPI_read(0, buf, blk_addr,blk_len) == 0)
	ret = USBD_OK;
 return ret;
 /* USER CODE END 6 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
 /* USER CODE BEGIN 7 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 if(USER_SPI_write(0, buf, blk_addr,blk_len) == 0)
	ret = USBD_OK;
 return ret;
 /* USER CODE END 7 */
}
 
/**
 * @brief .
 * @param None
 * @retval .
 */
int8_t STORAGE_GetMaxLun_FS(void)
{
 /* USER CODE BEGIN 8 */
 return (STORAGE_LUN_NBR - 1);
 /* USER CODE END 8 */
}
 
/* USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
/* USER CODE END PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
/**
 * @}
 */
 
/**
 * @}
 */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Thanks.

5 replies

Vangelis Fortounas
Associate II
April 11, 2021

hello

for the capacity question

 *block_num = hsd.SdCard.BlockNbr ;

 *block_size = hsd.SdCard.BlockSize;

for the second function ,

if device is ready, just return USBD_OK (0)

if not ready , return something else

ABatt.1
ABatt.1Author
Associate III
April 11, 2021

HI Vangelis,

hsd working for SDIO implementation, with BSP_SD generated from CUbeM.

I'm searcing for a SPI versione of this function.

Tesla DeLorean
Guru
April 11, 2021

STM32Cube_FW_F4_V1.24.0\Drivers\BSP\Adafruit_Shield\stm32_adafruit_sd.c

STM32Cube_FW_F4_V1.24.0\Drivers\BSP\STM32F4xx-Nucleo\stm32f4xx_nucleo.c

ADAFRUIT_TFT_JOY_SD_ID802

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ABatt.1
ABatt.1AuthorBest answer
Associate III
May 1, 2021

At the end I was succerfully writed the file.

Here is my usbd_stoge_if.c, writed based on user_diskio_spi.c an user_diskio_spi.h from https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : usbd_storage_if.c
 * @version : v1.0_Cube
 * @brief : Memory management layer.
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under Ultimate Liberty license
 * SLA0044, the "License"; You may not use this file except in compliance with
 * the License. You may obtain a copy of the License at:
 * www.st.com/SLA0044
 *
 ******************************************************************************
 */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "usbd_storage_if.h"
#include "C:\ST\Progetti\Test_USB_2\STM32CubeIDE\Application\User\FATFS\Target\user_diskio_spi.h"
 
/* USER CODE BEGIN INCLUDE */
 
/* USER CODE END INCLUDE */
 
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE END PV */
 
/** @addtogroup STM32_USB_OTG_DEVICE_LIBRARY
 * @brief Usb device.
 * @{
 */
 
/** @defgroup USBD_STORAGE
 * @brief Usb mass storage device module
 * @{
 */
 
/** @defgroup USBD_STORAGE_Private_TypesDefinitions
 * @brief Private types.
 * @{
 */
 
/* USER CODE BEGIN PRIVATE_TYPES */
 
/* USER CODE END PRIVATE_TYPES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Defines
 * @brief Private defines.
 * @{
 */
 
#define STORAGE_LUN_NBR 1
//#define STORAGE_BLK_NBR 0x10000
#define STORAGE_BLK_NBR 0x3AB780
#define STORAGE_BLK_SIZ 0x200
 
/* USER CODE BEGIN PRIVATE_DEFINES */
 
/* USER CODE END PRIVATE_DEFINES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Macros
 * @brief Private macros.
 * @{
 */
 
/* USER CODE BEGIN PRIVATE_MACRO */
 
/* USER CODE END PRIVATE_MACRO */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_Variables
 * @brief Private variables.
 * @{
 */
 
/* USER CODE BEGIN INQUIRY_DATA_FS */
/** USB Mass storage Standard Inquiry Data. */
const int8_t STORAGE_Inquirydata_FS[] = {/* 36 */
 
 /* LUN 0 */
 0x00,
 0x80,
 0x02,
 0x02,
 (STANDARD_INQUIRY_DATA_LEN - 5),
 0x00,
 0x00,
 0x00,
 'S', 'T', 'M', ' ', ' ', ' ', ' ', ' ', /* Manufacturer : 8 bytes */
 'P', 'r', 'o', 'd', 'u', 'c', 't', ' ', /* Product : 16 Bytes */
 ' ', ' ', ' ', ' ', ' ', ' ', ' ', ' ',
 '0', '.', '0' ,'1' /* Version : 4 Bytes */
};
/* USER CODE END INQUIRY_DATA_FS */
 
/* USER CODE BEGIN PRIVATE_VARIABLES */
 
/* USER CODE END PRIVATE_VARIABLES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Exported_Variables
 * @brief Public variables.
 * @{
 */
 
extern USBD_HandleTypeDef hUsbDeviceFS;
 
/* USER CODE BEGIN EXPORTED_VARIABLES */
 
/* USER CODE END EXPORTED_VARIABLES */
 
/**
 * @}
 */
 
/** @defgroup USBD_STORAGE_Private_FunctionPrototypes
 * @brief Private functions declaration.
 * @{
 */
 
static int8_t STORAGE_Init_FS(uint8_t lun);
static int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size);
static int8_t STORAGE_IsReady_FS(uint8_t lun);
static int8_t STORAGE_IsWriteProtected_FS(uint8_t lun);
static int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);
static int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);
static int8_t STORAGE_GetMaxLun_FS(void);
 
/* USER CODE BEGIN PRIVATE_FUNCTIONS_DECLARATION */
 
/* USER CODE END PRIVATE_FUNCTIONS_DECLARATION */
 
/**
 * @}
 */
 
USBD_StorageTypeDef USBD_Storage_Interface_fops_FS =
{
 STORAGE_Init_FS,
 STORAGE_GetCapacity_FS,
 STORAGE_IsReady_FS,
 STORAGE_IsWriteProtected_FS,
 STORAGE_Read_FS,
 STORAGE_Write_FS,
 STORAGE_GetMaxLun_FS,
 (int8_t *)STORAGE_Inquirydata_FS
};
 
/* Private functions ---------------------------------------------------------*/
/**
 * @brief Initializes over USB FS IP
 * @param lun:
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Init_FS(uint8_t lun)
{
 /* USER CODE BEGIN 2 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 	 if(USER_SPI_initialize(0) == 0){
	 ret = USBD_OK;
 }
 
 return ret;//(USBD_OK);
 /* USER CODE END 2 */
}
 
/**
 * @brief .
 * @param lun: .
 * @param block_num: .
 * @param block_size: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size)
{
 /* USER CODE BEGIN 3 */
 //****** TO_DO *********
 *block_num = STORAGE_BLK_NBR;
 *block_size = STORAGE_BLK_SIZ;
 return (USBD_OK);
 /* USER CODE END 3 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_IsReady_FS(uint8_t lun)
{
 /* USER CODE BEGIN 4 */
	 USBD_StatusTypeDef ret = USBD_FAIL;
	 if(USER_SPI_status(0) == 0){
		 ret = USBD_OK;
	 }
	 return ret;
 return (USBD_OK);
 /* USER CODE END 4 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_IsWriteProtected_FS(uint8_t lun)
{
 /* USER CODE BEGIN 5 */
 return (USBD_OK);
 /* USER CODE END 5 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
 /* USER CODE BEGIN 6 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 if(USER_SPI_read(0, buf, blk_addr,blk_len) == 0)
	ret = USBD_OK;
 return ret;
 /* USER CODE END 6 */
}
 
/**
 * @brief .
 * @param lun: .
 * @retval USBD_OK if all operations are OK else USBD_FAIL
 */
int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)
{
 /* USER CODE BEGIN 7 */
 USBD_StatusTypeDef ret = USBD_FAIL;
 if(USER_SPI_write(0, buf, blk_addr,blk_len) == 0)
	ret = USBD_OK;
 return ret;
 /* USER CODE END 7 */
}
 
/**
 * @brief .
 * @param None
 * @retval .
 */
int8_t STORAGE_GetMaxLun_FS(void)
{
 /* USER CODE BEGIN 8 */
 return (STORAGE_LUN_NBR - 1);
 /* USER CODE END 8 */
}
 
/* USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
/* USER CODE END PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
/**
 * @}
 */
 
/**
 * @}
 */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Thanks.

PLy.1
Associate
December 6, 2022

Thanks for your example! I was able to accomplish a similar task for my project thanks to it.

Best regards,

Phuoc