Skip to main content
SLapi.3
Associate
Feb 23, 2023 8:55 AM UTC
Question

Modify the .bin file of NetxDuo example called Nx_WebServer

I am working with AZURE RTOS and I have implemented an HTTP web server application following the application example called Nx_WebServer and prepared for the demo board STM32F429ZI-Nucleo.

The example uses files html, js, jpg, svg to create a web site. These files are written in the flash of the STM32F429 starting from address 0x08100000.

To write these files into the flash it is necessary to create the file web_demo.bin that is provided with the other files of the example.

Now I need to change some of the files of the Web Site (essentially index.html and dashboard.html) an so I have to regenerate the corresponding web_demo.bin, but I not able to do that.

Someone can help to do this step?

Thanks

PS: I have seen an other identical question did by an other community member (@agalindo) in the past, but that question did not have a satisfactory answer.

This topic has been closed for replies.

7 replies

Billy OWEN
ST Employee
Feb 24, 2023 2:50 PM UTC

Hi @SLapi.3​ 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

Regards,

Billy

SLapi.3
SLapi.3Author
Associate
Feb 24, 2023 4:09 PM UTC

Thanks, I've been looking for a solution for two days..

Regards

Simone

Haithem Rahmani
ST Employee
Feb 24, 2023 5:02 PM UTC

Hi, @SLapi.3​ 

I'll share a CLI tool that allows you to create the binary image.

stay tuned.

regards

Haithem.

SLapi.3
SLapi.3Author
Associate
Feb 25, 2023 11:07 AM UTC

Hi @Haithem Rahmani​ I hope you can help me. Or if you can't send me a tool, please give me the format of the .bin file compliant with the FileSystem readable by the Web Server of the NetXDuo Add-On.

Regards

Simone

Haithem Rahmani
ST Employee
Feb 25, 2023 1:01 PM UTC

@SLapi.3​ 

please check your private messages.

XZhu.3
Associate
Mar 29, 2023 11:33 PM UTC

Hi, @Haithem Rahmani​ 

can you also share the tool and detail how to create the web_demo.bin file? I am also working on sample project Nx_WebServer on board STM32F429ZI-Nucleo. I modified the dashboard.html and used the Keil FCARM to generate the bin. But after uploaded to 0x08100000 of the board, the application stop working and the fx_media_open() return 0x90.

Thanks,