Question
missing Standard Interface Requests implementation on STM32_USB_Device_Library :(
Posted on December 14, 2015 at 17:11
Hi,
\STM32Cube_FW_F3_V1.4.0\Middlewares\ST\STM32_USB_Device_Library\Core\Src\usbd_ctlreq.c The device doesn't pass the usb test (USB3CV Tool at http://www.usb.org/developers/tools/) because some mandatory functions in usb device described in USB Spec Rev2.0 aren't implemented. Thesestandard
functions should be present inside USBD_StdItfReq function in usbd_ctlreq.c file : USB_REQ_CLEAR_FEATURE, USB_REQ_SET_FEATURE, USB_REQ_GET_STATUS, USB_REQ_GET_INTERFACE, USB_REQ_SET_INTERFACE and the structure USBD_HandleTypeDef should handle the current alternate interface setting. My question is : should I implement this functions, myself ? if yes, on next library update, my work will be erased. if no, is a future release of this library expected in a few time ? Thanks for reply #usb-stm32