Skip to main content
Bob S
Super User
Jan 13, 2022 7:07 PM UTC
Question

Missing HardFault_IRQn values in CubeF4 v1.26.2 and CubeF7 v1.16.1 and 1.16.2

CubeF4 version 1.26.2 and CubeF7 version 1.16.1 and 1.16.2 are missing the enum value for HardFault_IRQn in all of the device specific include files (ex. stm32f429xx.h and stm32f746xx.h). It may be missing in earlier versions, I did not check. CubeMX does generate code for a HardFault_Handler().

This topic has been closed for replies.

2 replies

TDK
Jan 13, 2022 7:44 PM UTC

Not sure it's a bug as much as a design choice. I don't think it was ever there. What functionality is lacking as a result of it not being defined?

Most (all?) of the functions which that IRQn_Type as a parameter cannot take HardFault_IRQn (if it existed) as a value since you can't disable it or change its priority. Of course they can't take NonMaskableInt_IRQn either and it's defined.

Edit: although they exist in H7 CMSIS files so it's certainly inconsistent.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Bob S
Bob SAuthor
Super User
Jan 14, 2022 7:19 PM UTC

This doesn't affect any code generated from CubeMX. My custom fault handler code passes the fault/IRQ number to a common reporting/handling function. When porting my code from L4xx/G4xx to F7xx and F4xx CPUs I got compiler errors for the missing value. Yeah, it is a minor thing, but as you said, inconsistent with (at least) the L4, G4 and H7 files.