Skip to main content
Dat Tran
Senior II
Sep 24, 2026 3:57 PM UTC
Question

MicroPython source-level debugging on STM32C071 with only 24 KB RAM

We recently added support for STM32C071 to our free, MIT-licensed MicroPython Debugger for VS Code.

The interesting part is that the STM32C071 has only 24 KB of RAM and 128 KB of Flash, yet you can still use source-level debugging directly from VS Code.

Set a breakpoint in your MicroPython source, press F5, and debug the code running on the actual STM32 MCU.

The debugger supports:

  • Breakpoints
  • Step Over / Step Into / Step Out
  • Variable inspection
  • Watch
  • Call Stack
  • Break on exceptions
  • Continue / Pause

GitHub: https://github.com/ghi-electronics/micropython-vsc-extension

VS Code Marketplace: https://marketplace.visualstudio.com/items?itemName=ghielectronics.micropython-debugger

For testing, I used an STM32C071KBU6 running MicroPython with SPI and PWM on a DUELink Holiday Tree: Holiday Tree | DUELink

Here is example source: micropython-vsc-extension/examples/stm32c07/chrismastree_example at main · ghi-electronics/micropython-vsc-extension

I'm interested in hearing from other STM32 + MicroPython users — what STM32 device are you using, and what would you like to see supported?

1 reply

mƎALLEm
ST Technical Moderator
Sep 24, 2026 4:16 PM UTC

Hello ​@Dat Tran and thank you for your valuable assets/sharing.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.