Skip to main content
MJova.1
Associate II
Jan 21, 2021 3:15 PM UTC
Solved

MCU serial number

For some reasons it will be good to write my own MCU serial number for USB purpose.. Is it possible to change seria number of hte MCU and how to do this...

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Jan 22, 2021 11:00 AM UTC

Any number that is persistently stored on the device will do. Could be stored in flash, user option bytes, external eeprom etc.. Just implement the Get_SerialNum(void) function and supply your own variant of deviceserial0 and deviceserial1.

9 replies

Tesla DeLorean
Guru
Jan 21, 2021 3:20 PM UTC

No, but you can write your own code to generate the USB Serial number

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MJova.1
MJova.1Author
Associate II
Jan 22, 2021 10:39 AM UTC

Some explanation will be good... I found that into usbd_desc.c file is is generated but I am not sure how I can add my own serial number. Some useful explanation with example will be good.

Tesla DeLorean
Guru
Jan 22, 2021 12:21 PM UTC

It is putting an alpha/numeric identifier in a USB descriptor, how complicated can that be?​

​

Why isn't the current method working for you now?

​

I​f you want some linear number space, or particular form you have to manage the allocation and programming of each individual device.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Jan 22, 2021 12:29 PM UTC

If you need to uniquely serialized each device at final test most of the challenge is how you manage that allocation. On the STM32 side you'd likely want to put serialization, configuration, keys and calibration ​data into FLASH or OTP areas you have set aside for that purpose.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KnarfB
KnarfBBest answer
Super User
Jan 22, 2021 11:00 AM UTC

Any number that is persistently stored on the device will do. Could be stored in flash, user option bytes, external eeprom etc.. Just implement the Get_SerialNum(void) function and supply your own variant of deviceserial0 and deviceserial1.

Pavel A.
Jan 23, 2021 10:01 PM UTC

@KnarfB​ Are there any option bytes that are available for random user data? In which STM32 family?

Thanks,

Pavel

KnarfB
Super User
Jan 25, 2021 8:47 AM UTC

Not really/many, but they do exist. For example some F0 (RM0091) have 2 bytes of user data. That's okay for 2^16 boards.

On some F7 (RM0385) you may use BOOT_ADD1 for that, if the feature is not needed.