Skip to main content
NB_Saschen1
Associate
Mar 9, 2021 10:30 AM UTC
Solved

MCU is not waking up from STOP mode when it receives data over USART

Hi All,

I created a test project to Wake Up the device from STOP Mode when it receives data over UART.

I ported code from "UART_WakeUpFromStopUsingFIFO" available at /STM32Cube/Repository/STM32Cube_FW_L5_V1.3.1/Projects/STM32L562E-DK/Examples/UART/

Example project from STM is working as expected. The Device entered STOP Mode and Woke Up when it received data.

But, My test project is not working.

More Info:

1. The project was created for STM32L562 MCU.

2. Test board is L562-DK

3. LED GREEN is not turn ON in my project if USART 1 configured.

4. Wake Up from STOP Mode is not working.

5. Receving bytes over UART is working when I disabled the code to enter STOP Mode ( SystemClock_Config_fromSTOP() ) and Configure the system clock after wake up from STOP Mode ( SystemClock_Config_fromSTOP() ). USART 1 is used.

I have attached my project in zip file.

Can you advise me, how to resolve it?

Thanks

This topic has been closed for replies.
Jaroslav BECKA
Jaroslav BECKABest answer
ST Employee
Mar 16, 2021 11:35 AM UTC

Hello,

I've downloaded your project, tested it on nucleo-L552ZE-Q and was able to figure out the root cause of the problem.

The execution gets stuck after the first wake-up from STOP in HAL_RCC_OscConfig() called from SystemClock_Config_fromSTOP().

The while loop waiting for RCC_CR_PLLRDY ends with a timeout, since this flag is never set.

The execution then goes to Error_Handler().

A reason for that is a wrong PLL parameter passed in RCC_OscInitStruct, in particular RCC_OscInitStruct->PLL->PLLM is 1 in your case.

The correct value for the given configuration is 4.

The RCC_OscInitStruct values are obtained by calling the function HAL_RCC_GetOscConfig(), which is a previous step in SystemClock_Config_fromSTOP().

STM32 can wake-up from STOP mode with either MSI or HSI clock source. If a different clock settings is then used by the application (e.g. external clock source or PLL is used), the clock tree has to be re-configured after wake-up (that's why SystemClock_Config_fromSTOP() is called) .

In your project the internal HSI RC 16 MHz oscillator is used as wake-up source, see main():

  /* Specify HSI as the clock source used after wake up from stop mode */

  __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);

In the SystemClock_Config_fromSTOP() the PLL is turned on and the HSI is configured as PLL source.

However, when I check your SystemClock_Config() which is used for initial clock configuration (called at the beginning of main()),

a different internal oscillator is used, namely MSI. It is used as PLL source and all the PLL parameters are set accordingly.

When you then obtain the RCC_OscInitStruct values by calling the function HAL_RCC_GetOscConfig() in SystemClock_Config_fromSTOP(),

you get the values for MSI and not for HSI (so wrong PLL configuration values)!

These are then passed to HAL_RCC_OscConfig(&RCC_OscInitStruct).

This configuration (PLLSource = HSI, PLLM = 1, PLLN = 55, PLLR = 2) results in a frequency 440 MHz generated by the PLL, which is way higher than the CPU max. frequency 110 MHz.

With the correct configuration (PLLSource = HSI, PLLM = 4, PLLN = 55, PLLR = 2), the resulting frequency is 110 MHz (so CPU max.).

There are a few ways how to solve the problem, e.g.:

1) Add the following line in the SystemClock_Config_fromSTOP() just before the HAL_RCC_OscConfig(&RCC_OscInitStruct) call:

RCC_OscInitStruct.PLL.PLLM = 4;

2) Re-write the SystemClock_Config() function to use HSI instead of MSI and set the above parameters PLLSource = HSI, PLLM = 4, PLLN = 55, PLLR = 2 (preferable solution).

Of course, this is for the max. CPU frequency 110 MHz, if you want to use lower frequency, you can adjust the values.

I also recommend to add the two followin lines at the beginning of main():

 DBGMCU->CR &= ~DBGMCU_CR_DBG_STOP;

 DBGMCU->CR &= ~DBGMCU_CR_DBG_STANDBY;

This will disable debug in STOP and STANDBY modes. Some IDEs enable this feature automatically, afterwards the device will wake-up from STOP mode due to an SysTick interrupt (provided that SysTick is activated and its interrupt enabled). A power cycle might be needed to apply this configuration.

You can check these values during debug in DBGMCU->CR. But this is a different story.

I will upload the modified project.

Best regards

Jaroslav Becka

2 replies

Jaroslav BECKA
Jaroslav BECKABest answer
ST Employee
Mar 16, 2021 11:35 AM UTC

Hello,

I've downloaded your project, tested it on nucleo-L552ZE-Q and was able to figure out the root cause of the problem.

The execution gets stuck after the first wake-up from STOP in HAL_RCC_OscConfig() called from SystemClock_Config_fromSTOP().

The while loop waiting for RCC_CR_PLLRDY ends with a timeout, since this flag is never set.

The execution then goes to Error_Handler().

A reason for that is a wrong PLL parameter passed in RCC_OscInitStruct, in particular RCC_OscInitStruct->PLL->PLLM is 1 in your case.

The correct value for the given configuration is 4.

The RCC_OscInitStruct values are obtained by calling the function HAL_RCC_GetOscConfig(), which is a previous step in SystemClock_Config_fromSTOP().

STM32 can wake-up from STOP mode with either MSI or HSI clock source. If a different clock settings is then used by the application (e.g. external clock source or PLL is used), the clock tree has to be re-configured after wake-up (that's why SystemClock_Config_fromSTOP() is called) .

In your project the internal HSI RC 16 MHz oscillator is used as wake-up source, see main():

  /* Specify HSI as the clock source used after wake up from stop mode */

  __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);

In the SystemClock_Config_fromSTOP() the PLL is turned on and the HSI is configured as PLL source.

However, when I check your SystemClock_Config() which is used for initial clock configuration (called at the beginning of main()),

a different internal oscillator is used, namely MSI. It is used as PLL source and all the PLL parameters are set accordingly.

When you then obtain the RCC_OscInitStruct values by calling the function HAL_RCC_GetOscConfig() in SystemClock_Config_fromSTOP(),

you get the values for MSI and not for HSI (so wrong PLL configuration values)!

These are then passed to HAL_RCC_OscConfig(&RCC_OscInitStruct).

This configuration (PLLSource = HSI, PLLM = 1, PLLN = 55, PLLR = 2) results in a frequency 440 MHz generated by the PLL, which is way higher than the CPU max. frequency 110 MHz.

With the correct configuration (PLLSource = HSI, PLLM = 4, PLLN = 55, PLLR = 2), the resulting frequency is 110 MHz (so CPU max.).

There are a few ways how to solve the problem, e.g.:

1) Add the following line in the SystemClock_Config_fromSTOP() just before the HAL_RCC_OscConfig(&RCC_OscInitStruct) call:

RCC_OscInitStruct.PLL.PLLM = 4;

2) Re-write the SystemClock_Config() function to use HSI instead of MSI and set the above parameters PLLSource = HSI, PLLM = 4, PLLN = 55, PLLR = 2 (preferable solution).

Of course, this is for the max. CPU frequency 110 MHz, if you want to use lower frequency, you can adjust the values.

I also recommend to add the two followin lines at the beginning of main():

 DBGMCU->CR &= ~DBGMCU_CR_DBG_STOP;

 DBGMCU->CR &= ~DBGMCU_CR_DBG_STANDBY;

This will disable debug in STOP and STANDBY modes. Some IDEs enable this feature automatically, afterwards the device will wake-up from STOP mode due to an SysTick interrupt (provided that SysTick is activated and its interrupt enabled). A power cycle might be needed to apply this configuration.

You can check these values during debug in DBGMCU->CR. But this is a different story.

I will upload the modified project.

Best regards

Jaroslav Becka

NB_Saschen1
Associate
Mar 16, 2021 1:26 PM UTC

Hi Jaroslav,

Thanks for your reply.

Last week, I fixed this issue and I wanted to delete/close it but I was not able delete it.

Yesterday, I tried again to delete it but I got pop-up message "Admin not authorize you to delete" or something similar.

I should have added "This issue has been fixed".

Sorry for inconvenience caused.