Skip to main content
Giuseppe Cannarella
Associate II
July 20, 2017
Question

LwIP UDP stream max rate without packet loss

  • July 20, 2017
  • 0 replies
  • 827 views
Posted on July 20, 2017 at 12:19

Anyone can provide an example of STM32F437 FreeRTOS + LwIP UDP stream that no loose ethernet packets.

I've tried different implementation but, analyzing the ethernet packets, sometimes one packet is lost.

This is my implementation

void UDP_Send_Task(void const * argument)

{

  err_t error;   

 

  struct ip4_addr Sendtoipaddr;

 

  for (;;) 

  {   

    switch (Eth_MPX_Send_SM)

    {

      case CREATE_CONNECTION:

        IP4_ADDR(&Sendtoipaddr, 192, 168, 10, 124); 

        conn= udp_new();

        error = udp_bind(conn, IP_ADDR_ANY, 1234);

        if (error == ERR_OK)

        {

          PayloadCounter=0;

          Eth_MPX_Send_SM= SEND_PCKTS;//start to send pkcts

          //vTaskSuspend(NULL);

        }

      break;

      case SEND_PCKTS:         

        //HAL_GPIO_WritePin(LED5_GPIO_Port, LED5_Pin, GPIO_PIN_RESET);                       

        buf = pbuf_alloc(PBUF_TRANSPORT,sizeof(SendBuff),PBUF_REF);

       

        for (i=0; i<32; i=i+2)

        {

          SendBuff[i]= (PayloadCounter >>8)& 0xFF;

          SendBuff[i+1]= (uint8_t)PayloadCounter & 0xFF;

          PayloadCounter ++;

        }

       

        buf->payload = SendBuff;

       

        //memcpy (buf->payload, gbuf.mpx.buf, sizeof(gbuf.mpx.buf)); 

       

        TempBuf = buf->payload;

       

        First= ((uint16_t)TempBuf[0] <<8) | TempBuf[1];

        if (First != (Last+1))

        {

          ErrCount++;

        }

        Last= ((uint16_t)TempBuf[1022]<<8) | (uint16_t)TempBuf[1023];              

       

        error= udp_sendto(conn, buf, &Sendtoipaddr, 1234);

       

        if (error != ERR_OK)

        {

          NetErr++;             

        }

        //netbuf_free(buf);

        pbuf_free(buf); //De-allocate packet buffer

        vTaskDelay(pdMS_TO_TICKS(1));

        //NetDataAvailable =FALSE;

        //HAL_GPIO_WritePin(LED5_GPIO_Port, LED5_Pin, GPIO_PIN_SET);

        //vTaskSuspend(NULL);      

      break;

    }     

  } 

}

Thanks

#example #udp-test-tool #lwip #stm32f4 #udp #streaming
This topic has been closed for replies.