Skip to main content
ark2
Associate II
Nov 10, 2022 7:33 AM UTC
Question

lwip tcp server problem solution please

I made this sauce to implement lwip tcp server

If you try to remove the st-link wire and do it without debugging, the server itself doesn't work

I try to find a way, but I don't know where the problem is

If the LED on the board blinks, it means it's down

Is there a problem with why the server is not working?

If you turn it to debugging, you receive it without any problems, generate a message, and then send it

Then isn't there a problem with the sauce?

If the connection itself is not working when there is no debugging, I don't think the server is created

But if it's a circuit problem, I think it's weird to be a server when you debug it

I don't know where to look

When debugging, the client sent and received properly when it connected to the client from hercules or Raspberry Pi

void Tcp_Task(void const * argument)
 
{
 
 /* USER CODE BEGIN Tcp_Task */
 
 
 
 struct netconn *conn, *newconn;
 
 err_t err, accept_err;
 
 struct netbuf *buf;
 
 void *data;
 
 u16_t len;
 
 
 
 LWIP_UNUSED_ARG(argument);
 
 
 
 conn = netconn_new(NETCONN_TCP);
 
 
 
 if (conn!=NULL)
 
 { 
 
 // netconn_bind(conn, NULL, port 번호)
 
 err = netconn_bind(conn, NULL, 5001);
 
 
 
 if (err == ERR_OK)
 
 {
 
 netconn_listen(conn);
 
 
 
 while (1) 
 
 {
 
 accept_err = netconn_accept(conn, &newconn);
 
 
 
 if (accept_err == ERR_OK) 
 
 {
 
 while (netconn_recv(newconn, &buf) == ERR_OK) 
 
 {
 
 do 
 
 {
 
 netbuf_data(buf, &data, &len);
 
 memcpy(receivemsg, data, len);
 
 
 
 // 송신 메시지 �?성
 
 transmitmsg = procPacket();
 
 
 
 // 메시지 길�?�를 불러오는 함수
 
 msg_len = getsendPackSize();
 
 
 
 // 메시지 송신
 
 netconn_write(newconn, transmitmsg, msg_len, NETCONN_COPY);
 
 
 
 } 
 
 while (netbuf_next(buf) >= 0);
 
 
 
 netbuf_delete(buf);
 
 }
 
 netconn_close(newconn);
 
 netconn_delete(newconn);
 
 }
 
 
 
 osDelay(100);
 
 }
 
 }
 
 else
 
 {
 
 netconn_delete(newconn);
 
 }
 
 }
 
 
 
 
 
 /* Infinite loop */
 
 for(;;)
 
 {
 
 osDelay(100);
 
 }
 
 /* USER CODE END Tcp_Task */
 
}

This topic has been closed for replies.