Skip to main content
hobbyloseruser
Associate
October 1, 2025
Solved

LwIP not running properly on STM32H7S78-DK

 

Hey ST-Community,

I’m working with an STM32H7S78-DK board and trying to get Ethernet running. TouchGFX and FreeRTOS are working fine, but I’m stuck with lwIP. The task starts, but DHCP never succeeds (the printed IP is always 0.0.0.0). I also tried with a static IP, but I still can’t ping the board. Deactivating TouchGFX didn't help.

I've followed this video: STM32 : How to Get an IP Address via DHCP on STM32H7S78-DK with LwIP using IAR EWARM

LwIP has the following memory settings:

  1. MEM_SIZE = 14*1024Bytes
  2. TCPIP_THREAD_SIZE = 4 * 1024Bytes

I've configured the MPU as well following the given Video.

I’m not sure where to look next – maybe I’m missing some configuration step? Has anyone successfully used lwIP with this board and could give me a hint?

Thanks a lot in advance!

hobbyloseruser
hobbyloseruserBest answer
Associate
October 1, 2025

Hello, thanks a lot for the quick reply!

That really helped me fix the issue. In Wireshark I noticed that the whole DHCP sequence was missing, which led me to take a closer look at my configuration.

I was able to solve it by reconfiguring some ETH settings and adjusting the task priorities.

For anyone facing similiar issues:

  1. Double-check the ETH pinout and jumpers on your board against CubeMX.
  2. Ensure that the TouchGFX task has a higher priority than the lwIP tasks, otherwise the display might crash (at least for me).

 

Again, thanks a lot! ^^

4 replies

ST Employee
October 1, 2025

Hello @hobbyloseruser, and welcome to ST Community!

Could you try enabling DHCP, regenerating the project, and monitoring the traffic using a tool like Wireshark? This will help us determine if the DHCP four-step sequence—Discover, Offer, Request, Acknowledge (DORA)—is halting mid-communication or not occurring at all. Also, for DHCP to work, you need to connect your board either directly to your router or to your computer with a DHCP server running. Please check these points and get back to me with your feedback.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
GStou
Associate II
April 17, 2026

Dear STackPointer64,

I'm stuck with the same problem, but with me the display is not active. (another issue to solve)

I have set-up a monitoring of the DHCP process, which I had to initiate myself.


 struct dhcp *dhcp_data = netif_dhcp_data(&gnetif);
	 if (dhcp_data != NULL) {
	 printf("[DHCP] State: %d, Retries: %d\r\n", dhcp_data->state, dhcp_data->tries);
	 }​

Stuck in State 6

The orange LED is blinking, in line with the process waiting for an ACK.

Another computer directly get's an IP address using the same cable.

ST Employee
April 17, 2026

Hello @GStou,

Could you please create a new thread describing your issue in detail? This will help maximize visibility and make it easier for the community to follow and respond. please refer to How to write your question to maximize your chances to find a solution for best practices.

Please include:

  • The board or MCU you are using
  • The exact problem you are facing
  • Relevant code snippets or screenshots
  • Any steps you already tried

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
hobbyloseruser
hobbyloseruserAuthorBest answer
Associate
October 1, 2025

Hello, thanks a lot for the quick reply!

That really helped me fix the issue. In Wireshark I noticed that the whole DHCP sequence was missing, which led me to take a closer look at my configuration.

I was able to solve it by reconfiguring some ETH settings and adjusting the task priorities.

For anyone facing similiar issues:

  1. Double-check the ETH pinout and jumpers on your board against CubeMX.
  2. Ensure that the TouchGFX task has a higher priority than the lwIP tasks, otherwise the display might crash (at least for me).

 

Again, thanks a lot! ^^