Skip to main content
SSone.1
Associate II
Aug 4, 2025 4:11 PM UTC
Question

LwIP Custom memory pool configuration

I'm working on building an Ethernet infrastructure using LWIP on an STM32H7 series MCU for various purposes. In this setup, I want to avoid using malloc, and instead rely entirely on LWIP’s memory pool system for all memory allocations. Here's the configuration I’m planning to use:

MEM_LIBC_MALLOC 0 // Don't use the standard malloc (i.e., disable mem_malloc from libc)
MEMP_MEM_MALLOC 1 // Use mem_malloc for allocating MEMP pools
MEM_USE_POOLS 1 // Redirect mem_malloc calls to the defined memory pools
MEMP_USE_CUSTOM_POOLS 1 // Enable support for user-defined custom pools
MEM_USE_POOLS_TRY_BIGGER_POOL 1 // Allow searching for a larger pool if needed

In lwippools.h, I’ll define custom pools with different sizes like this:

 

LWIP_MALLOC_MEMPOOL_START
 LWIP_MALLOC_MEMPOOL(24, 128)
 LWIP_MALLOC_MEMPOOL(16, 256)
 LWIP_MALLOC_MEMPOOL(8, 512)
 LWIP_MALLOC_MEMPOOL(4, 1024)
 LWIP_MALLOC_MEMPOOL(4, 1536)
LWIP_MALLOC_MEMPOOL_END

 

For RX, I will use the following structure from STM's LWIP examples:

 

#define ETH_RX_BUFFER_CNT 8U
LWIP_MEMPOOL_DECLARE(RX_POOL, ETH_RX_BUFFER_CNT, sizeof(RxBuff_t), "Zero-copy RX PBUF pool");
__DMA_RAM extern u8_t memp_memory_RX_POOL_base[];

 

I have three questions:

  1. The following two options seem to contradict each other: MEMP_MEM_MALLOC = 1 and MEM_USE_POOLS = 1. Will this configuration work as I intend (i.e., using mem_malloc() but redirecting it to pools)?

  2. If it does work, do I still need the memory space defined by PBUF_POOL_SIZE? Can I set this to 0? In other words, does my configuration allow LWIP to use only the custom pools defined in lwippools.h instead of the default PBUF_POOL memory?

  3. In this configuration, will LWIP allocate MEMP_NUM_.. defined pool items (e.g., MEMP_NUM_TCP_PCB, MEMP_NUM_NETBUF, etc.) from the default static MEMP pools, or will those also be served from the custom pools defined in lwippools.h?

 

This topic has been closed for replies.

1 reply

ST Employee
Aug 6, 2025 12:28 PM UTC

Hello @SSone.1, and welcome to ST Community!

After reviewing the LwIP init.c file, the memp sanity checks show that MEMP_MEM_MALLOC and MEM_USE_POOLS cannot be used together. So, to answer your first two questions, no, it does not work that way. Regarding your third question, MEMP_NUM_* allocations come from custom pools, using the smallest pool that fits the required length.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.