Skip to main content
gdere.1
Associate
Oct 5, 2022 11:54 AM UTC
Question

LWIP: allocation fails in Heap (mem_malloc) for TX

Hello,

I'm on a STM32H743 (nucleo-H743ZI2), and I got LWIP (no OS) to "work", as in it receives ip packets and reads them. The problem is with allocating on the heap. I didn't use the libc_malloc option, the heap pointer is at 0x30044000 and is 1600 bytes long, and I configured the MPU for this area as follows:

MPU_InitStruct.Number = MPU_REGION_NUMBER2;
 MPU_InitStruct.BaseAddress = 0x30044000;
 MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

The problems I encounter are:

mem_malloc: could not allocate 60 bytes
etharp_raw: could not allocate pbuf for ARP request.

The ram stats before it shows

MEM HEAP
 
avail: 1600
 
used: 0
 
max: 0
 
err: 0

(And after it, it's the same but with the error counted)

Is my config ok?

This topic has been closed for replies.

2 replies

gdere.1
gdere.1Author
Associate
Oct 7, 2022 2:24 PM UTC

I think I found the reason: the HEAP isn't initialized with zeros

Robert Sexton
Associate II
Oct 7, 2022 5:17 PM UTC

This is a really small heap for lwIP. The input driver will allocate enough space to handle a full ethernet frame, and then you have buffers need for outgoing traffic. In my experience, you should start with about 8k worth of memory and go higher if your application requires it. ( lwipopts.h MEM_SIZE )

I've got an lwIP device on my desk that uses about 2k of heap (max) with trivial network activity.