Skip to main content
Associate II
May 7, 2024 1:13 PM UTC
Solved

LWIP

Hi,

how can I check if my client in connected to pc server?

--------------------------

/* init code for LWIP */

MX_LWIP_Init();

/* USER CODE BEGIN 5 */

LOCK_TCPIP_CORE();

tcp_setup();

UNLOCK_TCPIP_CORE();

---------------------------

void tcp_setup(void)

{

uint32_t data = 0xdeadbeef;

/* create an ip */

ip4_addr_t ip;

IP4_ADDR(&ip,192,168,1,4); //IP of my PHP server

/* create the control block */

testpcb = tcp_new(); //testpcb is a global struct tcp_pcb

// as defined by lwIP

/* dummy data to pass to callbacks*/

tcp_arg(testpcb, &data);

/* register callbacks with the pcb */

// tcp_recv(testpcb, tcpRecvCallback);

tcp_sent(testpcb, tcpSendCallback);

tcp_err(testpcb, tcpErrorHandler);

/* now connect */

tcp_connect(testpcb, &ip, 8888, connectCallback);

}

---------------------------

this snippet run and is OK.

How can I check if the client is alwais connected to pc server?

Can anyone help me?

Thank you in advance.

 

 

This topic has been closed for replies.
STeaBest answer
ST Employee
Jul 8, 2024 12:21 PM UTC

Hello @Stefano1 ,

To check if your client is always connected to the PC server, you can implement a mechanism to periodically send a "heartbeat" or "keep-alive" message from the client to the server. If the server does not receive this message within a certain timeframe, it can assume the client is disconnected. Similarly, the client can check for responses from the server to ensure the connection is still active.

here is an example:

#define KEEP_ALIVE_INTERVAL 5000 // 5 seconds

void keepAliveTimerCallback(void *arg) {
 if (testpcb != NULL) {
 // Send a keep-alive message
 tcp_write(testpcb, "KEEP_ALIVE", strlen("KEEP_ALIVE"), TCP_WRITE_FLAG_COPY);
 tcp_output(testpcb);
 }
 // Re-arm the timer
 sys_timeout(KEEP_ALIVE_INTERVAL, keepAliveTimerCallback, NULL);
}
void tcp_setup(void) {
...
 // Start the keep-alive timer
 sys_timeout(KEEP_ALIVE_INTERVAL, keepAliveTimerCallback, NULL);
}

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STeaBest answer
ST Employee
Jul 8, 2024 12:21 PM UTC

Hello @Stefano1 ,

To check if your client is always connected to the PC server, you can implement a mechanism to periodically send a "heartbeat" or "keep-alive" message from the client to the server. If the server does not receive this message within a certain timeframe, it can assume the client is disconnected. Similarly, the client can check for responses from the server to ensure the connection is still active.

here is an example:

#define KEEP_ALIVE_INTERVAL 5000 // 5 seconds

void keepAliveTimerCallback(void *arg) {
 if (testpcb != NULL) {
 // Send a keep-alive message
 tcp_write(testpcb, "KEEP_ALIVE", strlen("KEEP_ALIVE"), TCP_WRITE_FLAG_COPY);
 tcp_output(testpcb);
 }
 // Re-arm the timer
 sys_timeout(KEEP_ALIVE_INTERVAL, keepAliveTimerCallback, NULL);
}
void tcp_setup(void) {
...
 // Start the keep-alive timer
 sys_timeout(KEEP_ALIVE_INTERVAL, keepAliveTimerCallback, NULL);
}

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.