Skip to main content
SDall
Associate III
August 8, 2019
Question

Logico convert

  • August 8, 2019
  • 2 replies
  • 738 views

hi I have an encoder that has channel A channel B 5 volt output only and I wonder if it is possible to read gpio interrupt with a cortex m4 since it works at 3.3 volts? Do you need a logic level converter, some resistor or read it anyway?

This topic has been closed for replies.

2 replies

Bob S
Super User
August 8, 2019

Most pins on the STM32 family of parts are 5V compatible when used as input pins (like you would with the encoder). Check the data sheet for your processor, there is a chart that lists every pin and will show it as "FT" if it is 5V tolerant. Using pins as outputs they cannot drive above 3.3V, so some tricks or level shifting is needed. You might also look at the various timers on your chip as it is likely that at least one of them can be configured in "encoder" mode and do all/most of the work for you.

SDall
SDallAuthor
Associate III
August 8, 2019

Thanks​