Skip to main content
waclawek.jan
Super User
Jun 1, 2022 7:47 PM UTC
Question

[LL] Incorrect comment for VREFINT_CAL_VREF

In https://github.com/STMicroelectronics/STM32CubeL4/blob/c5e83f31696c3da4fb374224471afd08d9d457b3/Drivers/STM32L4xx_HAL_Driver/Inc/stm32l4xx_ll_adc.h#L346 the comment for VREFINT_CAL_VREF says

 /* Analog voltage reference (Vref+) value with which temperature sensor has been calibrated in production (tolerance: +-10 mV) (unit: mV). */

but it probably refers to the voltage reference with which VREFINT has been calibrated in production.

See also the same comment for TEMPSENSOR_CAL_VREFANALOG a couple of lines below.

#copypaste

JW

This topic has been closed for replies.

4 replies

Piranha
Principal III
Jun 1, 2022 10:08 PM UTC

I guess it's a "bug" report, because it's located in a source code... :)

waclawek.jan
Super User
Jun 1, 2022 10:43 PM UTC

This is a bug in source which results in flawless binary.

And even more so, as probably in all STM32 both voltages for the factory calibs are identical, so even if you follow the wrong comment, the result will be correct.

A bug nonetheless... :)

Jan

Amel NASRI
ST Technical Moderator
Jun 28, 2022 4:17 PM UTC

Hi @Community member​ ,

I reported this copy-paste effect:) internally, to be fixed.

Internal ticket number: 131065 (This is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jun 28, 2022 6:57 PM UTC

Thanks, Amel.

Jan

@Amel NASRI​