Skip to main content
Associate
Aug 22, 2024 11:16 AM UTC
Solved

LL Driver For I2C while integrating BN0086

Hi

I am using STM32L031F6 microcontroller and trying to read data from BNO086. The HAL driver i2c code is working fine but LL driver code doens't work. I want to use LL driver for i2c. Following is my LL driver code for reading and writing.
 
Read Function:
 
void LL_I2C_Master_Receive(uint8_t i2cAddr, uint8_t *aReceiveBuffer, uint16_t size)
{
uint32_t startTime = SysTick_Get(); // Get the current SysTick value
LL_I2C_HandleTransfer(I2C1, (i2cAddr<<1), LL_I2C_ADDRSLAVE_7BIT, size, LL_I2C_MODE_RELOAD, LL_I2C_GENERATE_START_READ);
if(LL_I2C_GetAddressMatchCode(I2C1) == i2cAddr << 1)
{
/* Verify the transfer direction, a write direction, Slave enters receiver mode */
if(LL_I2C_GetTransferDirection(I2C1) == LL_I2C_DIRECTION_READ)
{
/* Clear ADDR flag value in ISR register */
LL_I2C_ClearFlag_ADDR(I2C1);
}
else
{
/* Clear ADDR flag value in ISR register */
LL_I2C_ClearFlag_ADDR(I2C1);
}
}
else
{
/* Clear ADDR flag value in ISR register */
LL_I2C_ClearFlag_ADDR(I2C1);
}
 
// /* (2) Loop until end of transfer received (STOP flag raised) ***************/
while(!LL_I2C_IsActiveFlag_STOP(I2C1))
{
if(LL_I2C_IsActiveFlag_RXNE(I2C1))
{
aReceiveBuffer[ubReceiveIndex++] = LL_I2C_ReceiveData8(I2C1);
}
}
/* (3) Clear pending flags, Check Data consistency **************************/
LL_I2C_ClearFlag_STOP(I2C1);
}
 
Write function:
 
 
void LL_I2C_Master_Transmit(uint8_t i2cAddr, const uint8_t *pData, uint16_t size)
{
uint32_t startTime = SysTick_Get(); // Get the current time from SysTick or another timer
 
/* (1) Initiate a Start condition to the Slave device ***********************/
LL_I2C_HandleTransfer(I2C1, (i2cAddr << 1), LL_I2C_ADDRSLAVE_7BIT, size, LL_I2C_MODE_AUTOEND, LL_I2C_GENERATE_START_WRITE);
 
/* (2) Loop until end of transfer received (STOP flag raised) ***************/
while (!LL_I2C_IsActiveFlag_STOP(I2C1))
{
// Check TXIS flag value in ISR register to ensure we can transmit data
if (LL_I2C_IsActiveFlag_TXE(I2C1))
{
if (size > 0) // Ensure there is data left to transmit
{
LL_I2C_TransmitData8(I2C1, *pData++); // Transmit data
size--; // Decrease the number of bytes to transmit
}
}
}
 
/* (3) Clear pending flags, Data consistency are checking into Slave process */
LL_I2C_ClearFlag_STOP(I2C1); // Clear the STOP flag to complete the I2C communication
}
 
But the data is not properly Receiving, if any Mistake in these code? Does LL actually work with I2C?

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Aug 23, 2024 8:40 AM UTC

Sorry, I2C example with LL driver is for NUCLEO-L073RZ:

STM32CubeL0/Projects/NUCLEO-L073RZ/Examples_LL/I2C at master · STMicroelectronics/STM32CubeL0 · GitHub

 

For NUCLEO-L031K6 board, you can use the project LL template provided here:

STM32CubeL0/Projects/NUCLEO-L031K6/Templates_LL at master · STMicroelectronics/STM32CubeL0 · GitHub and follow the readme file to build your application.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

ST Technical Moderator
Aug 22, 2024 2:05 PM UTC

Hello @Anusree_k ,

You can follow the I2C examples (LL driver) provided in the STM32CubeL0 firmware package for the NUCLEO-L031K6 board:

STM32CubeL0/Projects/NUCLEO-L031K6/Examples/I2C at master · STMicroelectronics/STM32CubeL0 · GitHub

This will help you on your project implementation.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Anusree_kAuthor
Associate
Aug 22, 2024 4:24 PM UTC

Hello,

I didn't see the LL Driver under the link you suggested. I checked the link, but it uses HAL for the I2C. Could you please verify this?

Imen.DBest answer
ST Technical Moderator
Aug 23, 2024 8:40 AM UTC

Sorry, I2C example with LL driver is for NUCLEO-L073RZ:

STM32CubeL0/Projects/NUCLEO-L073RZ/Examples_LL/I2C at master · STMicroelectronics/STM32CubeL0 · GitHub

 

For NUCLEO-L031K6 board, you can use the project LL template provided here:

STM32CubeL0/Projects/NUCLEO-L031K6/Templates_LL at master · STMicroelectronics/STM32CubeL0 · GitHub and follow the readme file to build your application.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Aug 23, 2024 10:47 AM UTC

Hello @Anusree_k 

 

what is the size of the data to be read? 

The reload mode is used when the data size to be read is greater than 255, however it is mandatory to call LL_I2C_HandleTransfer with LL_I2C_MODE_AUTOEND mode for the last amount of data less than 255 bytes. 

 

please refer to this post for more details 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om