Skip to main content
OKose.1
Associate
Jul 27, 2022 1:27 PM UTC
Question

Lidar ethernet communication

Hi guys, my Lidar sensor named Livox Tele-15 communicates via ethernet. It gets IP by connecting to the modem in its own example application. It transfers data by connecting to IP in computer software. I want to control Lidar with a controller from STM32F7 series. Can I connect Lidar directly to STM controller via ethernet without using modem?

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Jul 27, 2022 1:30 PM UTC

The whole point of standards like ethernet, IP, etc is that they are hardware-independent.

So the Lidar's ethernet will connect to *any* other ethernet device.

You will have to study the Lidar's documentation to find exactly what protocols it supports over its ethernet, what API it provides, etc ...

Certainly, an STM32F7 can support ethernet comms.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.